First Littelfuse SiC MOSFET Provides Ultra-Fast Switching in Power Electronics

Combines ultra-low switching losses, high efficiency and superior robustness, even at high temperatures

Click to download a high resolution image:
1200V SiC MOSFETs Image

CHICAGO, October 2, 2017 — Littelfuse, Inc., the global leader in circuit protection, today introduced its first series of silicon carbide (SiC) MOSFETs, the latest addition to the company’s growing power semiconductor line. In March, Littelfuse took another incremental step towards establishing industry leadership in the power semiconductor industry through a majority investment in the well-respected SiC technology development company, Monolith Semiconductor Inc. The LSIC1MO120E0080 Series, with a voltage rating of 1200V and ultra-low (80mΩ) on-resistance, is the first organically designed, developed, and manufactured SiC MOSFETs to be released by this partnership. This device is optimized for high-frequency switching applications, providing a combination of ultra-low switching losses and ultra-fast switching speeds that’s unavailable with traditional power transistor solutions.

When compared with silicon devices that have the same rating, the SiC MOSFET Series enables substantially greater energy efficiency, reduced system size/weight, and increased power density in power electronics systems. It also offers superior robustness and exceptional performance, even at high operating temperatures (150°C).

Typical applications for these new SiC MOSFETs include power conversion systems such as solar inverters, switch mode power supplies, UPS systems, motor drives, high voltage DC/DC converters, battery chargers and induction heating.

“Our new SiC MOSFET Series is a critical milestone in our journey to become a leading component supplier in the power semiconductor industry,” said Michael Ketterer, product marketing manager for Power Semiconductors, Electronics Business Unit at Littelfuse. “Our SiC MOSFET application support network is prepared to help customers enhance the performance of their existing designs, as well as assist those developing new power converter products.”

The LSIC1MO120E0080 Series SiC MOSFET offers these key benefits:

  • Ultra-fast switching supports higher efficiency and increased power density.
  • Lower switching losses allow for higher switching frequencies.
  • Higher operating temperatures ensure greater device robustness in a wider array of high temperature applications.

LSIC1MO120E0080 Series SiC MOSFET is available in TO-247-3L packaging and provided in tubes in quantities of 450. Sample requests may be placed through authorized Littelfuse distributors worldwide. For a listing of Littelfuse distributors, please visit

For More Information
Additional information is available on the LSIC1MO120E0080 Series SiC MOSFET product page. For technical questions, please contact: Michael Ketterer, product marketing manager for Power Semiconductors, Electronics Business Unit,

About Littelfuse
Founded in 1927, Littelfuse is the world leader in circuit protection with growing global platforms in power control and sensing. The company serves customers in the electronics, automotive and industrial markets with technologies including fuses, semiconductors, polymers, ceramics, relays and sensors. Littelfuse has over 10,000 employees in more than 40 locations throughout the Americas, Europe and Asia. For more information, please visit