Application Design Center - Cell Phone

 

Circuit Protection of SIM Socket



Solutions

Design Notes:

Protection Application:
The signals used in the Subscriber Identification Module (SIM) circuit include Data, Clock and Reset. Since these are low-speed, low-voltage signals the capacitance of the suppressors is not a concern. The electrical threat is ESD.
Solution Description:
As shown at the left, discrete multilayer varistors can be used for board layout flexibility, or to reduce part count, a single TVS diode array can be used.
Companion Solutions:
Does not apply.
Regulatory Issues:
The IEC 61000-4-2 will be the most appropriate standard that applies for this port. It supplies a test method for verifying that the end product is not susceptible to ESD events.
Unique Features:
Does not apply.
Application Warnings:
Does not apply.