Application Design Center - Cordless Phone
Circuit Protection of Antenna
Solutions
Design Notes:
- Protection Application:
- The communication signals carried by the antenna operate in the radio frequency ranges of 900, 1,900 (DECT), 2,400 and 5,800 MHz, and are less than 1.0 Vp-p in magnitude. Due to the high frequency nature of these signals, the capacitance of the suppressor must be taken into account to avoid signal attenuation. The electrical threat will be ESD.
- Solution Description:
- As shown at the left, a single PulseGuard® suppressor is used to protect the antenna element.
- Companion Solutions:
- Does not apply.
- Regulatory Issues:
- The IEC 61000-4-2 will be the most appropriate standard that applies for this circuit. It supplies a test method for verifying that the end product is not susceptible to ESD events.
- Unique Features:
- Does not apply.
- Application Warnings:
- Does not apply.
.