Application Design Center - Desktop / Notebook
Circuit Protection of Dial-Up
Solutions
Design Notes:
- Protection Application:
- The signals carried on the tip and ring lines by dial-up circuits operate up to 56,000 bits/sec., so the capacitance of the protection device does not need to be controlled. The electrical threats include lightning surges and Power Cross conditions
- Solution Description:
- As shown at the left, a fuse or PTC can be used for Power Cross protection, and a SIDACtor® thyristor for lightning surge protection. The specific part numbers are determined by matching the operating voltage, and surge’s peak pulse current value to that of the surge suppressor.
- Companion Solutions:
- Does not apply.
- Regulatory Issues:
- In customer premises equipment like computers and set top boxes, there are a number of safety and performance-based Regulatory standards that apply. These include:
TIA-968
GR-1089
ITU K.20, K.21
UL 60950/EN 60950
- Unique Features:
- Does not apply.
- Application Warnings:
- Does not apply.