Application Design Center - Digital Still/Video Camera
Circuit Protection of Hard Disk Drive
Solutions
Design Notes:
- Protection Application:
- For internal hard disk drives, the drive resides within the chassis of the application. This precludes the user from contacting the data bus, so ESD is not expected to be a threat. On the power bus (typically 3.3VDC to 12VDC), the threats will be surge transients, ESD and overload currents.
- Solution Description:
- As shown at the left, an SMD chip fuse can be used for overload current protection, and a TVS diode or MLV for surge transients and ESD protection. The specific part numbers are determined by matching the power bus operating voltage to that of the suppressor.
- Companion Solutions:
- Does not apply.
- Regulatory Issues:
- The IEC 61000-4-2 will be the most appropriate standard that applies for this port. It supplies a test method for verifying that the end product is not susceptible to ESD events.
- Unique Features:
- Does not apply.
- Application Warnings:
- Does not apply.
.