Application Design Center - Cooktop- Electric (Resistive)
Circuit Protection of Power Supplies - AC mains
Solutions
Design Notes:
- Protection Application:
- Products that are directly connected to the AC mains (120 to 250VACrms) will be exposed to much more severe surge transients (lightning, load switching, etc.) and short circuit/overload conditions than on DC inputs. Because of this, the protection devices need to be more robust.
- Solution Description:
- As shown at the left (top), a cartridge or leaded fuse (5x20mm, 2AG, 3AG, TE5/TR5) can be used for short circuit and overload current conditions. For surge protection, an MOV (e.g. C-III, UltraMOV and LA series) with high energy handling capabilities should be used.
For products that also require electrical isolation between the hot and neutral lines and chassis (earth) ground, a GDT should be selected (left, bottom). The GDT is used to provide electrical isolation for the safety of the consumer.
- Companion Solutions:
- Does not apply.
- Regulatory Issues:
- Standards that specify safety and performance criteria include:
UL 6500/IEC 65065
UL1414
UL1449
- Unique Features:
- Does not apply.
- Application Warnings:
- Does not apply.
.