Application Design Center - IP Phone

 

Circuit Protection of Ethernet -- Power over Ethernet (PoE) Ports



Solutions

Design Notes:

Protection Application:
There are two basic ways of providing DC Power over an Ethernet Port. Shown in the top figure is a method known as "phantom power" that puts a common-mode voltage on the Tx and Rx pairs. The lower figure shows the use of the spare pairs fround in the RJ45 connector to provide power.
Solution Description:
The Tx and Rx pairs should be protected using the appropriate Ethernet protection scheme. The DC power port should be protected using the DC Input protection scheme.
Companion Solutions:
None.
Regulatory Issues:
IEEE standard 802.3af, UL 60950 or EN 60950, Telcordia GR-1089 may apply.
Unique Features:
None.
Application Warnings:
None.
.