Application Design Center - Wireless LAN Access Point
Circuit Protection of Antenna - WLAN
Solutions
Design Notes:
- Protection Application:
- The communication signals carried by the antenna operate at different radio frequency, depending on WLAN protocol – 2,400 MHz for 802.11b/g/n, 5,000 MHz for 802.11a; and are less than 1.0 Vp-p in magnitude. Due to the high frequency nature of these signals, the capacitance of the suppressor must be taken into account to avoid signal attenuation. The electrical threat will be ESD.
- Solution Description:
- As shown at the left, a single PulseGuard suppressor is used to protect the antenna element.
- Companion Solutions:
- Does not apply.
- Regulatory Issues:
- The IEC 61000-4-2 will be the most appropriate standard that applies for this circuit. It supplies a test method for verifying that the end product is not susceptible to ESD events.
- Unique Features:
- Does not apply.
- Application Warnings:
- Does not apply.
.