Press Release
New SP03-3.3 SPA(TM) Silicon Protection Array Offers Low Distortion Overvoltage Protection Solution for Broadband
Littelfuse expands SP03-x overvoltage suppresion product series2009-02-17 10:00:00
DES PLAINES, IL, February 17, 2009 – Littelfuse, Inc. (NASDAQ/NGS:LFUS) today announced an expansion to the SP03-x overvoltage suppression device series, designed for low distortion overvoltage protection of data lines and interface circuits in Ethernet, T3/E3, DS3, ADSL2+, and VDSL2+ systems. The new SP03-3.3BTG is RoHS compliant, provides higher surge rating and better clamping than competing devices, and offers a multi-element design that lowers capacitive losses compared to TVS devices alone.
The SP03-x series combine a transient voltage suppression (TVS) device with a diode rectifier bridge to provide both longitudinal (common mode) and differential protection in one package, suppressing both positive and negative voltage surges.
This design results in low insertion loss and a log-linear capacitive loading characteristic with respect to the signal voltage across the device. The result is reduced intermodulation (IM) distortion compared to typical solid-state protection solutions for high-speed data lines.
A low clamping voltage for both common mode and differential surge conditions means there is less stress on the protected equipment, and more robust equipment equates to longer life. Input capacitance at 1MHz is typically 16pF (25pF max.), resulting in low attenuation and better line balance for high-speed data.
The SP03-3.3BTG has a reverse standoff voltage of 3.3V, and clamps surges to 11.5V under 50A surge current conditions (15V at 100A surge).
With peak surge rating of 150A or 3300W (8/20µs waveform), SP03-3.3BTG meets the requirements of the following standards:
- Telcordia GR1089 (Intra-Building): 100A, 2/10µs waveform
- ITU K.20: Ipp = 40A, 5/310µs waveform
- IEC 61000-4-2 (ESD): 30kV (air), 30kV (contact)
- IEC 61000-4-5 (Lightning): 100A, 8/20µs waveform
Availability.
The SP03-3.3BTG is available in SO-8 (MS 012) Surface Mount Packaging. OEM samples are available from stock. Tape and reel orders typically ship 8-10 weeks ARO, and come in reel pack quantities of 2500 for efficient, low-cost circuit board installation.
For More Information on the SP03-3.3BTG and any of the Littelfuse broadband circuit protection products, or other overvoltage and overcurrent protection devices, visit the Littelfuse website at http://www.littelfuse.com or call the Littelfuse Technical Support line at 1-800-999-9445.
Click Here For Detailed Specification Information.
Click Here to Download a High Resolution Photo.
------------
For circuit protection application design ideas, please visit the new Application Design Center section of our web site.
If you have questions or require technical support please contact the Littelfuse technical support hotline at 1-800-999-9445.
------------
About Littelfuse
As the worldwide leader in circuit protection products and solutions with annual sales of $530.9 million in 2008, the Littelfuse portfolio is backed by industry leading technical support, design and manufacturing expertise. Littelfuse products are vital components in virtually every product that uses electrical energy, including automobiles, computers, consumer electronics, handheld devices, industrial equipment, and telecom/datacom circuits. Littelfuse offers Teccor®, Wickmann® and Pudenz® brand circuit protection products. In addition to its Des Plaines, Illinois, world headquarters, Littelfuse has sales, distribution, manufacturing and engineering facilities in Brazil, China, England, Germany, Hong Kong, India, Ireland, Japan, Korea, Mexico, the Netherlands, the Philippines, Singapore, Taiwan and the U.S. For more information, please visit Littelfuse’s web site at www.littelfuse.com.
"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995. Any forward looking statements contained herein involve risks and uncertainties, including, but not limited to, product demand and market acceptance risks, the effect of economic conditions, the impact of competitive products and pricing, product development and patent protection, commercialization and technological difficulties, capacity and supply constraints or difficulties, exchange rate fluctuations, actual purchases under agreements, the effect of the company's accounting policies, and other risks which may be detailed in the company's Securities and Exchange Commission filings.