Press Release

 

Littelfuse Introduces Ultra MOVTM 25S Varistor Series with High Peak Surge Current Ratings and High Energy Absorption Capability

The new varistor series withstands peak surge current up to 22 kA at single 8/20 µs pulse and can protect against lightning striking interference and abnormal power source.

2009-08-03 09:00:00

CHICAGO, Illinois, August 3, 2009 – Littelfuse (NASDAQ: LFUS) today announced the launch of Ultra MOVTM 25S Varistor Series for applications requiring high peak surge current rating and high energy absorption capability. The new varistor series withstands peak surge current up to 22 kA at single 8/20 µs pulse which is the highest in the market. It can protect against lightning striking interference and abnormal power source from incoming power lines.

The device in 25 mm X 25 mm square form in a radial lead package with straight leads is a new concept of circuit protection for high peak surge applications such as Surge Protective Devices (SPD), Uninterruptable Power Supplies (UPS), Transient Voltage Surge Suppression (TVSS) modular, non-modular TVSS, DIN rail TVSS, AC power taps, AC power meters, measuring and controlling systems, etc.

Ultra MOVTM 25S Varistor Series is characterized as having very fast response time with a wide range of operation voltages ranging from 115 VAC to 750 VAC. Phenolic coated option is available which makes possible operating temperature up to 125 °C and thus, can even prevent fire.

For more information, please visit the Littelfuse web site at www.littelfuse.com or contact your local Littelfuse technical support expert.

Click here for the product specifications

Click here for high resolution photo

------------

For circuit protection application design ideas, please visit the new Application Design Center section of the Littelfuse web site.

If you have questions or require technical support please contact the Littelfuse technical support hotline at 1-800-999-9445.


------------

About Littelfuse
As the worldwide leader in circuit protection products and solutions with annual sales of $531 million in 2008, the Littelfuse portfolio is backed by industry leading technical support, design and manufacturing expertise. Littelfuse products are vital components in virtually every product that uses electrical energy, including automobiles, computers, consumer electronics, handheld devices, industrial equipment, and telecom/datacom circuits. Littelfuse offers Teccor®, Wickmann® and Pudenz® brand circuit protection products. In addition to its Chicago, Illinois, world headquarters, Littelfuse has sales, distribution, manufacturing and engineering facilities in Brazil, China, England, Germany, Hong Kong, India, Ireland, Japan, Korea, Mexico, the Netherlands, the Philippines, Singapore, Taiwan and the U.S.

For more information, please visit Littelfuse’s web site at www.littelfuse.com.


"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995. Any forward looking statements contained herein involve risks and uncertainties, including, but not limited to, product demand and market acceptance risks, the effect of economic conditions, the impact of competitive products and pricing, product development and patent protection, commercialization and technological difficulties, capacity and supply constraints or difficulties, exchange rate fluctuations, actual purchases under agreements, the effect of the company's accounting policies, and other risks which may be detailed in the company's Securities and Exchange Commission filings.


Get the latest info