Press Release

 

Littelfuse Introduces SP3050 Series - Low Capacitance, Surge/Lightning Protection Array

Newest addition to the SPATM portfolio is designed to suppress large surge/lightning transients per IEC61000-4-5 with just 2pF of total capacitance.

2009-08-06 09:00:00

CHICAGO, Illinois, August 6, 2009 – Littelfuse, Inc. (NASDAQ/NGS: LFUS) today announced the introduction of the SP3050 Series, a four-channel diode array with an integrated zener diode.

The SP3050 series comes in a SOT23-6 package and provides a high level of protection against EOS threats such as ESD and surge/lightning for electronic devices.

It is particularly suitable for secondary or tertiary protection in 10/100/1000 Ethernet applications where surge/lightning transients are the main concern. Furthermore, the total capacitance of 2pF makes it usable in higher speed applications such as USB 2.0 where an enhanced level of ESD protection is often required.

The new SP3050 Series is RoHS compliant and complies with the following standards:

  • ESD, IEC61000-4-2, ±20kV (contact), ±30kV (air)
  • EFT, IEC61000-4-4, 40A (5/50ns)
  • Lightning, IEC61000-4-5, 10A (8/20µs)


  • The SP3050 device has a 6V reverse standoff voltage with extremely low leakage ≤1µA. Furthermore, it has a dynamic resistance under 0.7Ω that gives it an excellent clamping capability for ESD and surge/lightning transients.

    For more information about the SP3050 Series, please visit the Littelfuse website at www.littelfuse.com or contact your local Littelfuse Technical Support Expert. Click here for the product specifications

    Click here for high resolution photo

    ------------

    For circuit protection application design ideas, please visit the new Application Design Center section of the Littelfuse web site.

    If you have questions or require technical support please contact the Littelfuse technical support hotline at 1-800-999-9445.


    ------------

    About Littelfuse
    As the worldwide leader in circuit protection products and solutions with annual sales of $531 million in 2008, the Littelfuse portfolio is backed by industry leading technical support, design and manufacturing expertise. Littelfuse products are vital components in virtually every product that uses electrical energy, including automobiles, computers, consumer electronics, handheld devices, industrial equipment, and telecom/datacom circuits. Littelfuse offers Teccor®, Wickmann® and Pudenz® brand circuit protection products. In addition to its Chicago, Illinois, world headquarters, Littelfuse has sales, distribution, manufacturing and engineering facilities in Brazil, China, England, Germany, Hong Kong, India, Ireland, Japan, Korea, Mexico, the Netherlands, the Philippines, Singapore, Taiwan and the U.S.

    For more information, please visit Littelfuse’s web site at www.littelfuse.com.


    "Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995. Any forward looking statements contained herein involve risks and uncertainties, including, but not limited to, product demand and market acceptance risks, the effect of economic conditions, the impact of competitive products and pricing, product development and patent protection, commercialization and technological difficulties, capacity and supply constraints or difficulties, exchange rate fluctuations, actual purchases under agreements, the effect of the company's accounting policies, and other risks which may be detailed in the company's Securities and Exchange Commission filings.


    Get the latest info