Press Release

 

Littelfuse New 250V Miniature Fuse/Clip Assembly Enables Easy Circuit Board Level Fuse Replacement

New 160 Series surface mount fuse/clip assembly offers high inrush current withstand capability and ability to replace fuses without exposing the circuit board and other components to the risks of rework solder heat

2009-08-13 09:00:00

CHICAGO, Illinois, August 13, 2009 – Littelfuse (NASDAQ: LFUS) announces today the launch of the 160 Series 250V time-lag surface mount fuse/clip assembly device for over-current protection of printed circuit boards. The 160 Series is suitable for applications requiring both high current withstand capability for unpredictable low pulse/surge currents as well as quick and easy field replacement of blown fuse. It is RoHS compliant and Halogen-free.

In a dimension of approximately 10.90 mm (L) X 4.80 mm (W) X 4.80 mm (H), the 160 Series fuse offers the current ratings from 500mA to 5A, with a maximum inrush current withstand (I2t ) of 127A2secs and an interrupting rating of 50A at 250VAC. The fuse clip holder lowers the probability of fuse opening during momentary overloads. The fuse clip holder also makes possible field replacement of fuse which brings down rework and maintenance cost brought by the warranty on board replacements. As an intangible benefit, the field replaceable feature also avoids exposing other sensitive components to the risks of reworking and excessive soldering heat.

This fuse/clip assembly was designed particularly for LED lighting, lighting system, power converter and adaptor as well as telecom equipment. This product complements the broad line of Littelfuse surface mount fuses used on secondary side of power circuits, with ratings from 62mA to 15A at voltages from 24V to 350V.

The 160 Series is available in tape and reeled packaging, orders typically take 4-6 weeks ARO.

For additional specification information and to request samples, please visit the Littelfuse web site at www.littelfuse.com/series/160.html or contact your local Littelfuse Technical Support Expert. Click here for the product specifications

Click here for high resolution photo

------------

For circuit protection application design ideas, please visit the new Application Design Center section of the Littelfuse web site.

If you have questions or require technical support please contact the Littelfuse technical support hotline at 1-800-999-9445.


------------

About Littelfuse
As the worldwide leader in circuit protection products and solutions with annual sales of $531 million in 2008, the Littelfuse portfolio is backed by industry leading technical support, design and manufacturing expertise. Littelfuse products are vital components in virtually every product that uses electrical energy, including automobiles, computers, consumer electronics, handheld devices, industrial equipment, and telecom/datacom circuits. Littelfuse offers Teccor®, Wickmann® and Pudenz® brand circuit protection products. In addition to its Chicago, Illinois, world headquarters, Littelfuse has sales, distribution, manufacturing and engineering facilities in Brazil, China, England, Germany, Hong Kong, India, Ireland, Japan, Korea, Mexico, the Netherlands, the Philippines, Singapore, Taiwan and the U.S.

For more information, please visit Littelfuse’s web site at www.littelfuse.com.


"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995. Any forward looking statements contained herein involve risks and uncertainties, including, but not limited to, product demand and market acceptance risks, the effect of economic conditions, the impact of competitive products and pricing, product development and patent protection, commercialization and technological difficulties, capacity and supply constraints or difficulties, exchange rate fluctuations, actual purchases under agreements, the effect of the company's accounting policies, and other risks which may be detailed in the company's Securities and Exchange Commission filings.


Get the latest info