Press Release
New SP3002-04UTG Silicon Protection Array Offers Enhanced ESD Protection in a Small Form Factor Package
Latest addition to the existing SP3002 Series (SPATM) is offered in a space efficient, low profile 1.6 x 1.6 x 0.5 mm µDFN-6 package.2009-09-14 09:00:00
CHICAGO, Illinois, September 14, 2009
– Littelfuse, Inc. (NASDAQ/NGS:LFUS), today announced a package expansion of the SP3002 Series, a four channel diode array with an integrated zener diode. The µDFN-6 and SOT23-6 package options will be added to the existing SP3002 Series which previously consisted of only the SC70-6. All options provide enhanced ESD protection per IEC61000-4-2 for electronic devices with a very low input capacitance of 0.85pF.
The SP3002-04UTG is particularly suitable for high speed port protection in mobile devices or in any application where board space comes at a premium. The SP3002-04UTG offers a 43% space savings over the SC70-6 and a 68% savings over the SOT23-6.
The new SP3002-04UTG is RoHS compliant and complies with the following standards:
● ESD, IEC61000-4-2, ±12kV (contact), ±15kV (air)
● EFT, IEC61000-4-5, 40A (5/50ns)
● Lightning, IEC61000-4-5, 4.5A (8/20µs)
The SP3002 Series has a 6V reverse standoff voltage with extremely low leakage of <1µA. Furthermore, its low capacitance of 0.85pF combined with a low dynamic resistance of 1.1Ω, makes it an ideal choice to protect sensitive chipsets.
For more information about Littelfuse and our circuit protection products, please visit the Littelfuse web site at www.littelfuse.com or contact the Littelfuse Technical Support Team in your region.
Click here for the product specifications
Click here for high resolution photo
------------
For circuit protection application design ideas, please visit the new Application Design Center section of the Littelfuse web site.
------------
About Littelfuse
As the worldwide leader in circuit protection products and solutions with annual sales of $531 million in 2008, the Littelfuse portfolio is backed by industry leading technical support, design and manufacturing expertise. Littelfuse products are vital components in virtually every product that uses electrical energy, including automobiles, computers, consumer electronics, handheld devices, industrial equipment, and telecom/datacom circuits. Littelfuse offers Teccor®, Wickmann® and Pudenz® brand circuit protection products. In addition to its Des Plaines, Illinois, world headquarters, Littelfuse has sales, distribution, manufacturing and engineering facilities in Brazil, China, England, Germany, Hong Kong, India, Ireland, Japan, Korea, Mexico, the Netherlands, the Philippines, Singapore, Taiwan and the U.S.
For more information, please visit Littelfuse’s web site at www.littelfuse.com.
"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995. Any forward looking statements contained herein involve risks and uncertainties, including, but not limited to, product demand and market acceptance risks, the effect of economic conditions, the impact of competitive products and pricing, product development and patent protection, commercialization and technological difficulties, capacity and supply constraints or difficulties, exchange rate fluctuations, actual purchases under agreements, the effect of the company's accounting policies, and other risks which may be detailed in the company's Securities and Exchange Commission filings.