Press Release
Littelfuse New SM7 Series Surface Mount MOV Provides both Overvoltage Protection and Transient Suppression with Wide Operating Voltage up to 510 VAC
Its surface mount packaging, reflow solderability, high operating voltage and halogen-free features make it incomparable to other offerings in the market2009-10-12 09:00:00
CHICAGO, Illinois, October 12, 2009
– Littelfuse, Inc. (NASDAQ/NGS:LFUS), ) announces today the introduction of SM7 Series surface mount MOV for over-voltage protection and transient suppression. It is designed for continuous operation across AC power lines and is highly suitable for AC power meters, detectors & sensors, plug-in cards and remote controllers.
“Featured with wide operating voltage up to 510 VAC, SM7 Series provides the highest operating voltage among other similar offerings in the market,” explained Dave Lesperance, Director of Ceremic and Polymer Products Business of Littelfuse Inc. “On top of being lead-free and RoHS compliant, it is also Halogen-free which is not available in other similar offerings. “
“Reflow solderability is another key feature of this new product,” added Dave. “SM7 is a plastic-encapsulated surface mount MOV in a nylon molded package with tin-plated terminal which is fully qualified in lead-free and SnPb soldering and available for both reflow and wave soldering process.” SM7 is based on radial 7mm internal varistor element. Its operating ambient temperature is high as 85°C with peak pulse current of 1200A. SM7 Series is also UL recognized and has UL agency approval under UL 1449 edition 3.
The SM7 Series is available now for order and sample request through authorized Littelfuse distributors worldwide.
For more information about Littelfuse and our circuit protection products, please visit the Littelfuse web site at www.littelfuse.com or contact your local Littelfuse Technical Support Team.
Click here for high resolution photo
------------
For circuit protection application design ideas, please visit the new Application Design Center section of the Littelfuse web site.
If you have questions or require technical support please contact the Littelfuse technical support hotline at 1-800-999-9445.
------------
About Littelfuse
As the worldwide leader in circuit protection products and solutions with annual sales of $531 million in 2008, the Littelfuse portfolio is backed by industry leading technical support, design and manufacturing expertise. Littelfuse products are vital components in virtually every product that uses electrical energy, including automobiles, computers, consumer electronics, handheld devices, industrial equipment, and telecom/datacom circuits. Littelfuse offers Teccor®, Wickmann® and Pudenz® brand circuit protection products. In addition to its Chicago, Illinois, world headquarters, Littelfuse has sales, distribution, manufacturing and engineering facilities in Brazil, China, England, Germany, Hong Kong, India, Ireland, Japan, Korea, Mexico, the Netherlands, the Philippines, Singapore, Taiwan and the U.S.
For more information, please visit Littelfuse’s web site at www.littelfuse.com.
"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995. Any forward looking statements contained herein involve risks and uncertainties, including, but not limited to, product demand and market acceptance risks, the effect of economic conditions, the impact of competitive products and pricing, product development and patent protection, commercialization and technological difficulties, capacity and supply constraints or difficulties, exchange rate fluctuations, actual purchases under agreements, the effect of the company's accounting policies, and other risks which may be detailed in the company's Securities and Exchange Commission filings.