Product News Press Release
 

Littelfuse Announces High-Energy Series of Transient Voltage Suppressors to Protect Critical Equipment

New TVS diode devices are rated for up to 15kA surge current to protect against high-energy transients



2010-09-15 09:00:00

CHICAGO, IL, September 2, 2010 – Littelfuse, Inc. (NASDAQ/NGS:LFUS) has introduced its AK15 Series of Transient Voltage Suppressor (TVS) devices to prevent the destruction of expensive electronic gear from high-energy transients. With their 15kA (8x20 μs pulse)surge current rating, AK15 devices provide the highest level of TVS protection available in the industry. They will be especially useful to manufacturers of mission critical equipment such as cellular telecom infrastructure apparatus, industrial transient voltage surge suppression (TVSS) systems, railway trackside signaling circuitry, highway traffic control signals, and other industrial control equipment. The AK15 Series was designed to provide protection against transients generated by nearby lightning strikes and high-level voltage surges that occur on electrical lines when large industrial equipment is switched on and off.

The AK15 Series are bi-directional devices for use in equipment connected to AC electrical lines, but are also suitable for DC circuit protection. This Series utilizes Littelfuse’s exclusive Foldbak™ technology, which lowers clamping voltage levels below the TVS device’s avalanche state, which provides a higher level of protection. Their sharp breakdown voltage provides a fast response to electrical line transients. A 15kA rating means that electronic OEMs no longer have to gang multiple silicon avalanche diodes to get the level of protection they need. The ultra-compact design of the AK15 Series has 12-times less volume than traditional discrete device solutions. This simplifies circuit design configurations and testing, eliminates component insertion and connection errors on printed circuit boards, and reduces overall manufacturing costs. It also means that protection circuits have lower capacitance and resistance, leading to higher operating efficiencies.

Because the AK15 Series are silicon devices with glass passivated chip construction, they have no inherent wear-out mechanism when operated within their 15kA rating. This high-reliability design is UL Recognized, halogen-free, and RoHS compliant.

Availability

AK15 Series samples are available now for order and sample request through authorized Littelfuse distributors worldwide. AK15 devices are available 8-10 weeks ARO in 56 quantity bulk packs.


For more information about the AK15 Series, please visit the Littelfuse web site at www.littelfuse.com or contact your local Littelfuse Technical Support expert.
Click here for AK15 Series product specifications
Click here for high resolution photo

------------

For circuit protection application design ideas, please visit the new Application Design Center section of the Littelfuse web site.

If you have questions or require technical support please contact the Littelfuse technical support hotline at 1-800-999-9445.


------------

About Littelfuse
As the worldwide leader in circuit protection products and solutions with annual sales of $430.1 million in 2009, the Littelfuse portfolio is backed by industry-leading technical support, design and manufacturing expertise. Littelfuse products are vital components in virtually every product that uses electrical energy, including automobiles, computers, consumer electronics, handheld devices, industrial equipment and telecom/datacom circuits. Littelfuse offers Teccor®, Wickmann® and Pudenz® brand circuit protection products. In addition to its Chicago, Illinois, world headquarters, Littelfuse has sales, distribution, manufacturing and engineering facilities in Brazil, Canada, China, England, Germany, Hong Kong, India, Japan, Korea, Mexico, the Netherlands, the Philippines, Singapore, Taiwan and the U.S.

For more information, please visit Littelfuse’s web site at www.littelfuse.com.


"Safe Harbor" Statement under the Private Securities Litigation Reform Act of 1995. Any forward looking statements contained herein involve risks and uncertainties, including, but not limited to, product demand and market acceptance risks, the effect of economic conditions, the impact of competitive products and pricing, product development and patent protection, commercialization and technological difficulties, capacity and supply constraints or difficulties, exchange rate fluctuations, actual purchases under agreements, the effect of the company's accounting policies, and other risks which may be detailed in the company's Securities and Exchange Commission filings.


Stay Informed

Get the latest
product news, circuit
protection design tips
and best practices.