Overcurrent Circuit Protection: Fuse vs. PTC

PTC Protection Function
The principles of operation for a fuse have been documented over the years and are generally well understood. The actual process by which the PTC provides overcurrent circuit protection is less clear and merits further discussion. So far the PTChas been identified as being polymer based, current limiting and resettable.

The PTCs under discussion are conductive polymer based products. The polymer material used contains particles of carbon black as the conductive media. The resistance is controlled by the amount of carbon black introduced into the mixture. Heat produces some expansion of the polymer which causes the carbon black to shift resulting in less conductivity or an increase in resistance.

The PTC functions by current limiting a potentially damaging overcurrent to a safe level. Specifically the excessive current through the device causes internal heating (I2R) which raises the temperature of the PTC and results in an increase in its resistance. The resistance of the PTC is generally a small part of the total circuit impedance until the heating takes place. The increase in resistance for a polymer based PTC is nonlinear as shown in the graph below and this relatively large increase in resistance will reduce or limit the circuit current to a safe level. The transition from low to high resistance is referred to as the trip point.

The heat generated by this limited current through the higher resistance value will maintain the temperature of the PTCat a level that will cause the resistance to remain high. This thermal equilibrium condition will continue until power is removed from the circuit which allows the PTC to cool down and the resistance will decrease. The resettable feature of the PTC is based on the fact that the increase in resistance resulting from the increase in temperature is reversible. The PTC is reset or returned to the lower resistance state by removing the power from the circuit which allows the device to cool down. The unit is then ready to react to future overloads. The resistance will remain low if the cause of the overcurrent has been corrected but if the overcurrent recurs the device will again switch to the high resistance state.

More information about Resettable Fuses  

Get the latest info