Arc-Flash Calculator - Flash Boundary
Flash Protection Boundary
IEEE 1584 defines the Flash Protection Boundary as: “An approach limit at a distance from live parts that are uninsulated or exposed within which a person could receive a second degree burn." The accepted incident energy level is 1.2 Cal/Cm². NFPA 70E also defines the following related terms: