Arc-Flash Calculator - Fuse

Fuses

600 Volts and Below
In establishing fuse opening times for use in IEEE 1584 calculations over 300 tests were made using Class RK1 fuses from 30 through 600 amperes and Class L fuses from 601 through 2000 amperes. Section 9.13 of IEEE 1584 states: “Fuses from one manufacturer were used, but results with other manufacturers’ fuses of the same class should be similar.”
In addition, IEEE TRANSACTIONS ON INDUSTRY APPLICATIONS, VOL. 36, NO. 6, NOVEMBER/DECEMBER 2000 1741 The Use of Low-Voltage Current-Limiting Fuses to Reduce Arc-Flash Energy states in part:

“II. CURRENT-LIMITING FUSE DATA In order to determine the performance of current-limiting fuses, fuse manufacturers typically perform single-phase bolted-fault fuse tests based on the UL (U.S.)/CSA (Canada)/ANCE (Mexico) tri-national 248 series of standards. Note that the 248 series of standards calls out the maximum let-through values so that all fuses listed to the standard will have a uniform maximum let-through which can be utilized by equipment manufacturers and designers.”

Littelfuse fuses with short-circuit characteristics (opening times) consistent with fuses used in the IEEE tests include: LLNRK, LLSRK, LLSRK_ID, KLNR, and KLSR series (Class RK1); JTD, JTD_ID, and JLS series (Class J); KLPC and KLLU series (Class L); JLLN and JLLS series (Class T); and CCMR, KLDR, and KLKR series (Class CC).
Fuses not covered by the test date include: Class RK5, Class K5 ('One-Time'), and Class H (Renewable) fuses. These types of fuses do not provide the degree of arc-fault protection as the fuses listed above. It is recommended that Class RK5, K5, and H be replaced with a suitable fuse having better short-circuit characteristics.  


Stay Informed

Get the latest
product news, circuit
protection design tips
and best practices.