Arc-Flash - Precautions
The fundamental rule required by OSHA regulations is to completely deenergize all parts of an electrical system that may be exposed while working on it. Exposed, as it applies to live parts, means capable of being touched or approached nearer than a safe distance by a person. It applies to parts that are not properly guarded, isolated, or insulated. Covered parts are not considered insulated.
OSHA lockout/tagout procedures must be completed before opening any enclosure that may contain exposed electrically energized components. Only a qualified worker may then open the enclosure after donning the appropriate level of PPE as determined by the Flash Hazard Analysis. All exposed live parts must then be tested to insure that the equipment is in an electrically safe condition. There are only two exceptions to this rule. See: Understanding and Reducing Arc-Flash Hazards .
NFPA 70E places the responsibility on the employer to qualify employees who may be required to work on energized equipment and to train unqualified persons in any electrical safety-related practices that are necessary for their safety.
The information contained on this CD is believed to be accurate. However, it is provided solely to help the user determine incident energy and accompanying arc-flash hazard. Since the user determines input values and other circuit variables, Littelfuse expressly disclaims liability for any omissions or errors in the software, or results of calculations or analysis. All arc-flash calculations, including those in NFPA 70E, are based on a number of empirical decisions. Results obtained by using various calculators may not be identical due to different rounding of numbers, and selection of different opening times for protective devices. When faced with options, Littelfuse has attempted to select those values that result in higher incident energy. At best, all calculating methods and results only provide a guide for determining the level of PPE required. NFPA 70E cautions that additional developmental testing is required and calculation methods may require future revision.
The Littelfuse program calculates the incident energy, minimum required level of Personal Protective Equipment (PPE), and Flash Protection Boundary and Hazard Risk Category. These factors are an important part of the Arc-Flash Hazard Analysis required by and described in NFPA 70E. A complete Arc-Flash Hazard Analysis should help you increase employee safety and meet the requirements of NFPA 70E, NFPA 70 “National Electrical Code,” and OSHA Standards 29-CFR, Part 1910. Occupational Safety and Health Standards. 1910 sub part S (electrical) Standard number 1910.333 “Standards for Work Practices."
In addition, users are cautioned that the program only determines incident energy under specified test conditions used in IEEE 1584. The recommended level of PPE is the minimum recommended to reduce injury from burns that could occur from an arcing fault. Workers may still receive burns while wearing PPE. Burns from arc-flash are only one of the hazards of an arcing fault. Other potential hazards include: Direct and indirect pressure from arc blast, toxic vapors from copper and metallic coatings, vaporized insulation, which may release chlorine or other toxic gases, and particles of copper or other materials propelled by arc blasts. Actual shock hazards must also be considered. These factors need to be included in the documented plans for working on energized circuits.
While parts of the Standards, Regulations, and Codes especially relating to arc-flash hazards are quoted or summarized herein, readers are cautioned that only the complete Standards constitute the law or regulation and all parts must be followed where applicable.
In performing an Arc-Flash Hazard Analysis users are required to make a number of empirical decisions regarding available fault current, distance from the arc, etc. They are cautioned that choices made should reflect the most conservative values that will produce the maximum arc-flash conditions. These choices are further described and explained in the calculator.
An Overview of Arc-Flash Hazards is contained in Littelfuse Document: Understanding and Reducing Arc-Flash Hazards located on this CD. It is highly recommended that this paper be studied before using the calculator.
In addition, some critics take the position that calculating methods contained in the standards greatly understate the incident energy for systems under 600 volts. A question has also been raised concerning the effect conductor orientation has on direction and magnitude of arc blast. Additional testing is under consideration. The standards and regulations establish minimum requirements for improving safety. These minimums may not be adequate, and it may be necessary to use PPE with higher ratings than calculated.
OSHA lockout/tagout procedures must be completed before opening any enclosure that may contain exposed electrically energized components. Only a qualified worker may then open the enclosure after donning the appropriate level of PPE as determined by the Flash Hazard Analysis. All exposed live parts must then be tested to insure that the equipment is in an electrically safe condition. There are only two exceptions to this rule. See: Understanding and Reducing Arc-Flash Hazards .
NFPA 70E places the responsibility on the employer to qualify employees who may be required to work on energized equipment and to train unqualified persons in any electrical safety-related practices that are necessary for their safety.
The information contained on this CD is believed to be accurate. However, it is provided solely to help the user determine incident energy and accompanying arc-flash hazard. Since the user determines input values and other circuit variables, Littelfuse expressly disclaims liability for any omissions or errors in the software, or results of calculations or analysis. All arc-flash calculations, including those in NFPA 70E, are based on a number of empirical decisions. Results obtained by using various calculators may not be identical due to different rounding of numbers, and selection of different opening times for protective devices. When faced with options, Littelfuse has attempted to select those values that result in higher incident energy. At best, all calculating methods and results only provide a guide for determining the level of PPE required. NFPA 70E cautions that additional developmental testing is required and calculation methods may require future revision.
The Littelfuse program calculates the incident energy, minimum required level of Personal Protective Equipment (PPE), and Flash Protection Boundary and Hazard Risk Category. These factors are an important part of the Arc-Flash Hazard Analysis required by and described in NFPA 70E. A complete Arc-Flash Hazard Analysis should help you increase employee safety and meet the requirements of NFPA 70E, NFPA 70 “National Electrical Code,” and OSHA Standards 29-CFR, Part 1910. Occupational Safety and Health Standards. 1910 sub part S (electrical) Standard number 1910.333 “Standards for Work Practices."
In addition, users are cautioned that the program only determines incident energy under specified test conditions used in IEEE 1584. The recommended level of PPE is the minimum recommended to reduce injury from burns that could occur from an arcing fault. Workers may still receive burns while wearing PPE. Burns from arc-flash are only one of the hazards of an arcing fault. Other potential hazards include: Direct and indirect pressure from arc blast, toxic vapors from copper and metallic coatings, vaporized insulation, which may release chlorine or other toxic gases, and particles of copper or other materials propelled by arc blasts. Actual shock hazards must also be considered. These factors need to be included in the documented plans for working on energized circuits.
While parts of the Standards, Regulations, and Codes especially relating to arc-flash hazards are quoted or summarized herein, readers are cautioned that only the complete Standards constitute the law or regulation and all parts must be followed where applicable.
In performing an Arc-Flash Hazard Analysis users are required to make a number of empirical decisions regarding available fault current, distance from the arc, etc. They are cautioned that choices made should reflect the most conservative values that will produce the maximum arc-flash conditions. These choices are further described and explained in the calculator.
An Overview of Arc-Flash Hazards is contained in Littelfuse Document: Understanding and Reducing Arc-Flash Hazards
In addition, some critics take the position that calculating methods contained in the standards greatly understate the incident energy for systems under 600 volts. A question has also been raised concerning the effect conductor orientation has on direction and magnitude of arc blast. Additional testing is under consideration. The standards and regulations establish minimum requirements for improving safety. These minimums may not be adequate, and it may be necessary to use PPE with higher ratings than calculated.