SCCR Center

Welcome to the Littelfuse SCCR Center!


The 2005 National Electrical Code (NEC) [Article 409.110] addresses the need to accurately identify and label an industrial control panel's Short Circuit Current Rating (SCCR). This requirement is necessary to ensure the integrity of the panel and the safety of personnel during a short circuit situation.

The NEC also requires an SCCR for: Industrial machinery electrical panels [Article 670] Multiple motor HVAC equipment [Article 440] Meter disconnect switches [Article 230] Multiple motor controllers [Article 430] personnel during a short circuit situation.

Article 409 was added due to the dangerous and common misconception by equipment manufacturers that the circuit breaker's interrupting capacity or the fuse's interrupting rating in the panel's feeder circuit is also the panel's SCCR. In reality, the panel's SCCR is directly related to the current-limiting capabilities (opening time) of the protective device in the feeder circuit and the individual panel components' SCCR. In most cases, a panel's SCCR is less than the interrupting capacity or interrupting rating of the overcurrent device. personnel during a short circuit situation.

How is a panel's SCCR determined? NEC Article 409.110(3) states that the SCCR shall be based on a listed (i.e. UL tested) assembly or an approved method of calculation. The NEC further states that UL508A Supplement SB is an example of an approved method. To help clarify everything, Littelfuse POWR-GARD Products has created a number of tools listed below to help the equipment builder understand SCCR and learn how to maximize a panel's rating. personnel during a short circuit situation.

Also, keep in mind that an existing panel being moved to a new location within a facility still requires verification that its SCCR is greater than the new available fault current. As the panel is moved closer to the electrical service, the available fault current can increase, and the panel needs to withstand this new level. Even if the panel isn't moved and the available fault current increases from the utility company, this verification needs to be done to ensure a safe environment. personnel during a short circuit situation.

 
Increasing Safety and Reliability Using Current Limitation PF982
High SCCRs for Littelfuse Power Distribution Blocks
Littelfuse offers Power Distribution Blocks with high SCCRs in response to 2005 NEC Article 409 and UL 508A marking requirements for industrial control panels. This brochure shows the higher SCCRs for each Littelfuse Power Distribution Block part number.
SCCR Online Tutorial
Watch and listen to a 15-minute overview on how fuses can be used to increase the SCCR rating of an industrial control panel.
Littelfuse SCCR Presentation
This 43-slide presentation is designed to educate users about the new NEC and UL requirements for identifying and marking a industrial control panel with its corresponding Short-Circuit Current Rating (SCCR). Work through an example, and learn how fuses can be used to increase the SCCR for a given panel.
Using Current-Limiting Fuses to Increase SCCR of Industrial Control Panels - PF992
This 16-page brochure reviews NEC and UL 508A requirements and methods for determining SCCRs of industrial control panels. Learn how fuses can be used to increase these short circuit current ratings and improve worker safety.
Getting it straight: interruption rating vs. short-circuit current rating_PF977
Increasing Safety and Reliability Using Current Limitation PF982

Get the latest info