Reducing Arc-Flash with Resistance Grounding

How to modify your electrical system to eliminate 95% of Arc-Flash events

Learn How To:
  • Identify hazardous conditions caused by ground faults
  • Significantly reduce Arc-Flash Hazards with resistance grounding
  • Convert a solidly grounded or ungrounded system to resistance grounded
  • Maintain operations while preventing electrical faults
Who Should Attend:
  • Plant Managers & Plant Electrical Safety Managers
  • Electrical Maintenance Managers & Electrical System Designers
  • Electrical Contractors with Industrial Clients

The electrical industry is reevaluating strategies that prevent Arc Flash. Long used in mines, petro-chem, and other heavy industrial plants, resistance grounding has won converts in general industry. This proven systemic approach eliminates phase-to-ground Arc Flash incidents throughout an entire system.

Most Arc Flash events, even phase-to-phase, begin as ground faults. If the neutral point of a transformer connects to earth ground via a power resistor, the resistance limits phase-to-ground current to just a few amps; not enough to cause downtime by tripping the overcurrent protection device, and not enough to allow an Arc Flash hazard to occur. As a result this approach eliminates 95% of all Arc Flash incidents, according to IEEE.

Tony Locker, P.E. of Littelfuse is the presenter of this Webcast moderated by Plant Engineering's editor Bob Vavra.

You will be redirected to the webinar once you fill out the form