Solidly Grounded Systems

Due to the problem of ungrounded systems, a shift in philosophy occurred and designs moved from ungrounded to grounded systems. In most cases, the type of grounding system chosen was solidly grounded. A solidly grounded system is a system of conductors in which at least one conductor or point is intentionally grounded (usually the neutral point of transformer or generator windings). The problem with the direct connection is that ground fault current can be excessive, causing Arc-Flash hazards, extensive equipment damage, and possible injury to personnel.

Solidly Grounded System Example

FIGURE 5

  • In a solidly grounded system, the wye point (or neutral) of the power source is connected solidly to ground and offers a very stable system that maintains a fixed phase-to-ground voltage.
  • The high ground-fault current is easy to detect with fuses, circuit breakers, or protection relays, allowing for selective tripping (tripping the faulted feeder and not the main feeder).
  • When a ground fault occurs, high point-of-fault damage can quickly result since the energy available to the ground fault is only limited by the system impedance (which is typically very low).
  • Due to excessive ground-fault current and Arc-Flash Hazards, the faulted feeder must be removed from service. This does not allow for continuous operation during a ground fault.

Figure 6 illustrates an example of the dangers associated with solidly grounded systems. In this example, a ground-fault occurs and the overcurrent protection is set at 600 A.

Solidly Grounded System Example 2

FIGURE 6

  • Assume that this ground-fault is not a bolted fault, but an arcing fault due to an insulation breakdown or a partial reduction of clearances between the line and ground.
  • Because of the arc resistance, the fault current may be reduced to as low as 38% of the bolted-fault level. The fault current can be in the range of a normal load or a slight overload.
  • The fault current may be low enough that the overcurrent device (600-A circuit breaker) does not sense the fault current, or may pick it up but not trip for a long time.
  • The energy being supplied by the source is concentrated at the arc and could cause severe equipment damage very quickly. This energy release could cause a fire that in turn, could damage the premises and present an extreme hazard to personnel.


Aside from converting this solidly grounded system to resistance grounding, the best way to prevent damage is to detect low-level ground leakage prior to it becoming a ground fault. In order to accomplish this, the protection relay must be able to sense a low-level ground leakage without nuisance tripping.

In modern facilities, equipment often generates noise or harmonics that may interfere with a protection relay’s ability to function properly. For example, the noise or harmonics may be higher than the desired ground-fault relay settings, causing the relay to falsely operate when there is no fault on the system. The protection relay must be able to filter out noise or harmonics to provide reliable protection.

 
Generator Ground-Fault Relay

Sensitive Ground-Fault Relay

Ground-Fault Relay