Ungrounded ac systems, shown below, were used where continuity of power was critical. For example, chemical plants or refineries involving processes that cannot be interrupted without extensive dollar or product loss may have an ungrounded system. However, experience has proven that these systems are problematic and are being replaced with resistance grounded systems. Two major problems with ungrounded systems are transient overvoltages and difficulty locating ground faults.

FIGURE 4
- An ungrounded system has no point in the system that is intentionally grounded (other than the normal bonding which is always present to connect the non-current-carrying metal parts to ground). Grounding occurs only through system capacitance to ground (as shown in Figure 4).
- Continuity of power occurs because the system can operate with one phase faulted to ground.
- An intermittent or arcing fault can produce high transient overvoltages to ground. These voltages are impressed on the phase conductors throughout the system until the insulation at the weakest point breaks down. This breakdown can occur at any point in the electrical system, causing a phase-to-ground-to-phase fault.
- Although a ground fault can be detected or alarmed on the system, there is no way to determine the location of the fault.
- There are two methods used to detect ground faults in ungrounded systems. One method is to monitor the voltages between the phases and ground. As a ground fault develops, the faulted phase will collapse to ground potential, causing an indicator light to dim. The indicator lights on the unfaulted phases become brighter.
- A better method to detect a ground fault is to measure the insulation resistance. As the insulation deteriorates, a relay continuously monitoring the insulation resistance can alarm at different levels for predictive maintenance. A visual indication or meter can also be used.
|