Current and Voltage Unbalance, Phase Loss, Phase Reverse
Phase loss is also referred to as single phasing. When a phase loss occurs, negative-sequence current is equal to the positive-sequence current and unbalance is 100%. In this condition, one motor winding attempts to do the work of three, inevitably leading to overheating.
Phase reversal causes the negative-sequence current and voltage to be greater than the positive-sequence current and voltage. Voltage-based protection is advantageous to prevent a start with incorrect sequence. In some applications attempting to spin the motor backwards will result in damage to the load. An example of this is certain impeller designs in downhole pumps.
Solution: Modern motor protection relays use digital signal analysis to measure true-sequence components. These sequence components are used for thermal model calculations and take the extra heating into consideration. Voltage unbalance which drives current unbalance can be used as a start inhibit. Sequence components are also used for calculating unbalance, phase loss and phase reversal.