Ground Faults

Ground faults are the most common fault and can lead to more serious problems. Ground-fault protection, described elsewhere in this text, is an important consideration in motor loads.



Solution: The motor protection relay should be able to detect low-level ground-fault current when used on a resistance-grounded system.

 
PGR-6150 Motor Protection System

Motor Protection Relay

Motor Protection System