High Resistance Winding Faults
Winding-to-winding and winding-to-ground failures inside the motor are difficult to detect using the phase and ground-fault CTs due to low magnitudes of current.
Solution: Differential protection in high-end motor protection relays use multiple CTs to compare the current entering and leaving the winding. If there is a difference in currents then leakage is occurring. This sensitive protection is used on very large motors.
Solution: Differential protection in high-end motor protection relays use multiple CTs to compare the current entering and leaving the winding. If there is a difference in currents then leakage is occurring. This sensitive protection is used on very large motors.