Motor Jogging
NEMA designed motors are rated for two starts from cold and one start from hot per hour. Motor jogging refers to excessive starts and can cause overheating. The motor may not get up to full speed and the forced air cooling is not effective.
Solution: Since the thermal model accurately tracks the motor’s used thermal capacity at all times, including during starts and between starts, the starts-per-hour feature may not be required.
It is included for compatibility with protection relays that do not have dynamic thermal-modeling capability.