Overcurrent, Jam and Undercurrent

Overcurrent faults, also referred to as short circuits, can cause catastrophic motor failures and fires. Overcurrents can be caused by phase-to-phase and phase-to-ground-to-phase faults. A mechanical jam, such as a failed bearing or load, can cause locked-rotor current to be drawn by the motor, resulting in overheating.

Undercurrent protection is required by some codes as a safety measure. A water pump that cavitates can be dangerous. The water typically provides pump cooling. Without the cooling water, case temperature can reach an extremely high value. If valves are opened under these conditions and cold water is allowed to reach red-hot metal parts, the resulting steam pressures can destroy the pump and pose a serious personnel hazard.

Solutions: A multifunction motor protection relay has multiple trip and alarm settings for current protection. Overcurrent protection is typically set above locked rotor current and has a minimal delay time. Overcurrent protection may be used to trip a breaker instead of a starter due to the high fault levels. Jam protection is set below overcurrent and has a slightly longer delay time. Jam protection prevents motor heating that would otherwise lead to an overload trip. Jam protection is enabled after the motor is running to avoid tripping on starting current. Undercurrent is set below full-load current to detect loss of load.

 
Electronic Overload Relay

PGR-6150 Motor Protection System

Motor Protection Relay

Motor Protection System