Under and Overvoltage

Overvoltages cause insulation stress and premature breakdown. Undervoltages, such as those caused by brownouts, can lead to increased motor heating. Torque developed by an electric motor changes as the square of the applied voltage. A 10% reduction in voltage results in a 19% reduction in torque. If the motor load is not reduced, the motor will be overloaded.



Solution: Under and overvoltage protection are features found in a higher-end motor-protection relays. Voltage protection can be used proactively to inhibit a start.

 
Motor Protection Relay

Motor Protection System