littelfuse-about-us-news-jpg

Littelfuse Launches Worlds Smallest Subminiature Flange Mount Reed Sensors for Various Applications

59155 and 59156 Flange Mount Reed Sensors

Ideal for appliances, security/access control, and factory automation where space is limited

CHICAGO, August 10, 2023 -- Littelfuse, Inc.(NASDAQ: LFUS), an industrial technology manufacturing company empowering a sustainable, connected, and safer world, announced the release of its newest products, the 59155 and 59156, which are the world’s smallest subminiature flange mount reed sensors. The sensors' design provides compact size, contactless activation, and customization options, making them suitable for a wide range of tight-spacing applications across different industries.

Littelfuse introduces the most miniature flange-mount type reed sensor available in the market, measuring only 12.70 mm x 9.00 mm x 3.00 mm (0.500" x 0.354" x 0.118") with normally open contacts. The sensors can switch 120 Vac / 170 Vdc at 10 W. The case design allows mounting with an M2 screw at 0.1 Nm torque maximum or adhesive mounting.

The 59155 and 59156 sensors are available with wires exiting from the left-hand or right-hand side, making them ideal for use in many applications, including:

  • small appliances,
  • major appliances,
  • security and access control,
  • factory automation,
  • process equipment,
  • proximity and limit sensing, and
  • other IoT proximity sensing applications.

The new reed sensors provide a customizable, space-saving design to meet different installation requirements. Contactless activation prevents exposure to humidity or dust, improving the end equipment's lifetime.

“We understand the challenges that come with limited space in many applications, which is why we developed one of the world's smallest reed sensors,” said Ryan Sheahen, Global Market Manager at Littelfuse. “This extends our leadership in offering (one of the) the broadest and most comprehensive portfolio of magnetic sensing solutions to meet our customers’ needs.”

The 59155 and 59156 sensors compete with similar-sized products currently available on the market. However, the new Littelfuse sensors are slightly smaller while providing higher switching capability. They also have a wider operating temperature range, which is -40 °C to +105 °C, compared to others that offer -20 °C to +85 °C.

Availability

The 59155 and 59156 Reed Sensors are available in several sensitivity and cable length configurations. Place sample requests through authorized Littelfuse distributors worldwide. For a listing of Littelfuse distributors, please visit Littelfuse.com.

For More Information

Additional information on the latest series release is available on the 59155 and 59156 Reed Sensors product page. For technical questions, please contact Julius Venckus, Global Product Manager, EBU at jvenckus@littelfuse.com.

About Littelfuse

Littelfuse is a diversified, industrial technology manufacturing company empowering a sustainable, connected, and safer world. Across more than 20 countries, and with approximately 18,000 global associates, we partner with customers to design and deliver innovative, reliable solutions. Serving over 100,000 end customers, our products are found in a variety of industrial, transportation, and electronics end markets—everywhere, every day. Headquartered in Chicago, Illinois, United States, Littelfuse was founded in 1927. Learn more at Littelfuse.com.