リテルヒューズ-会社概要-ニュース-JPG

Carling Technologies、AVHシリーズ密閉型アンチバンダルプッシュボタンスイッチを改良

PLAINVILLE, September 14, 2023 - Carling Technologies, a Littelfuse, Inc. (NASDAQ: LFUS) brand, announced improvements to its AVH-Series sealed anti-vandal pushbutton switches. Available with dependent LED illumination, the feature can now be configured in one of two ways. The first is to have the ring-style LED on whenever the specified output is on. The second is to have the LED on whenever the mechanical latching switch is on.

"Some motors, even after power is removed, will act as a generator to keep the LED lit as it slowly stops rotating. The option to have the LED on when the mechanical latching switch is on eliminates that issue," said Jerry Peplau, Product Manager. "In addition to the new LED illumination option, we've made several updates to the design that will improve our customers' overall experience using these popular switches."

The AVH-Series illuminated switches are often used in security panels, public transit systems, traffic signals, emergency phones, industrial controls, and marine and outdoor applications.

What Else is New and Improved on the AVH-Series?

The AVH-Series is a high-current pushbutton switch available with ratings up to 30 A. Known for its safety and performance capabilities, it is well-suited for momentary, latching, NAV-ANCHOR, and dual output applications.

In addition to the new LED illumination option, the AVH-Series features the following improvements:

  • Led+ terminal can come out via a red wire for end-user wiring
  • Will not trip off if the load is disconnected via an external switch
  • New black ground wire eliminates miswiring of the ground tab and allows use as a drop-in replacement
  • No false trips due to a momentary drop in battery+ or ground when another unrelated circuit is energized

While the AVH-Series must be used in a circuit that has a fuse or circuit breaker of the correct amperage, it features an integrated thermal cutoff for safety in case of overheating.

For backfeed protection, the use of an external diode is still required.

Learn More About AVH-Series Sealed Anti-Vandal Pushbutton Switches

More information on AVH-Series illuminated sealed pushbutton switches can be found at: https://www.carlingtech.com/pushbutton-switches-av-avh-series

Requests for the AVH-Series can be placed through Carling authorized distributors and sales representatives worldwide. For a listing of distributors and sales representatives, please visit carlingtech.com.

About Carling Technologies

As a global leader in circuit protection, switching, and power distribution, Carling Technologies, a Littelfuse brand, is dedicated to developing modern, innovative solutions that ensure the communications technology, transportation, and infrastructure we rely on every day is safe, sustainable, and working when it matters most. As a part of Littelfuse since 2021, Carling Technologies has leveraged complementary engineering capabilities, application expertise, and product portfolios to provide greater value to its diverse OEM and distributor customer base. Learn more at carlingtech.com.

リテルヒューズ会社案内

リテルヒューズ(ナスダック:LFUS)は、工業技術を生み出すメーカー企業として、持続可能で接続性の高い、より安全な世界を実現します。世界20ヵ国以上に約18,000名の従業員を擁するリテルヒューズは、お客様への支援を通して革新的かつ信頼性の高いソリューションの設計と供給に取り組んでいます。顧客数 100,000 を超える当社の製品は、工業、輸送、エレクトロニクスといった各種市場のあらゆる場所で日々利用されています。 Learn more at littelfuse.com.