ࡱ> q` GbjbjqPqP 8::G>PPPPPPPd8(Dl d,4D(lllGGGbdddddd$+hPGGPPll&PlPl\PP\l( 03(<B994\9P\HGˤ^)LuGGG.dGGGdd$(.$5cD5dd.cdddPPPPPP ENGINEERING SPECIFICATION SYMCOM MODEL 777-LR-P Solid State Overload Relay GENERAL REFERENCES UL 508 Industrial Control Equipment Underwriters Laboratories IEC 60947 Low Voltage Switchgear and Controlgear International Electrotechnical Commission CSA C22.2 No. 14 Industrial Control Equipment Canadian Standards Association ANSI/IEEE C62.41 American National Standards Institute/Institute of Electrical & Electronics Engineers MODBUS over Serial Line Specification and Implementation Guide V1.02 UL 1053 Ground-Fault Sensing and Relaying Equipment Underwriters Laboratories Relays shall be installed according to the latest version of the National Electrical code. WARRANTY Manufacturer Warranty: The manufacturer shall guarantee the overload relay to be free from material and workmanship defects for a period of five years from the date of manufacture when installed and operated according to the manufacturers requirements. PRODUCTS MANUFACTURERS The equipment specified shall be the Model 777-LR-P, manufactured by SymCom, Inc. DESCRIPTION Regulatory Requirements: The equipment shall be UL Listed as type NKCRIndustrial Control Equipment-Motor Controllers-Auxiliary Devices. The equipment shall be cUL Listed as type NKCR7Industrial Control Equipment-Motor Controllers-Auxiliary Devices Certified for Canada. The equipment shall be CE marked for use in the European Union and evaluated against IEC 60947 Low Voltage Switchgear and Controlgear. The equipment shall be CSA certified as class 3211-03Industrial Control Equipment-Motor Controllers-Auxiliary Devices. Performance/Design Criteria: 777-LR-P 3-PHASE SOLID STATE OVERLOAD RELAY Protective Relay Functions The equipment shall provide protection against the following conditions: voltage single-phase/phase loss phase reversal low voltage high voltage voltage unbalance rapid cycling to prevent on-off cycling of the motor multiple times in rapid succession under current over current current unbalance current single-phase/phase loss low control voltage, to trip the motor if the average voltage falls below the low voltage setpoint x the low control voltage percentage, for the duration of the low control voltage trip delay ground fault contact failure, to trip the motor, if the motor starter is damaged which causes a current single-phase. Communication Capabilities The equipment shall include a Modbus interface when used with the SymCom Model RS485MS-2W or a DeviceNetTM interface when used with a SymCom Model COM-DN-P or CIO-DN-P, or a Profibus interface when used with SymCom Model CIO-777-PR. The equipment interface shall have the capability of connecting to the following systems: MMI (Man Machine Interface) SCADA (Supervisory Control and Data Acquisition) programs. DCS (Distributed Control System) PLC (Programmable Logic Controllers) SymCom Model RM-1000 Modbus remote display SymCom Model RM-2000 Modbus remote display The equipment shall support the following communication parameters: 9600 baud, Even parity, and 1 stop bit 9600 baud, Odd parity, and 1 stop bit 9600 baud, No parity, and 1 stop bit 19200 baud, Even parity, and 1 stop bit 19200 baud, Odd parity, and 1 stop bit 19200 baud, No parity, and 1 stop bit The equipment shall provide set points that are readable and writable via the Modbus/DeviceNetTM interface. The equipment shall provide the ability to energize and de-energize the motor via the Modbus/DeviceNetTM interface. The equipment shall provide a 10-second Modbus network watchdog to trip the relay when Modbus communication is lost. The equipment shall provide two programmable Modbus assemblies for reading large blocks of data. Network Capabilities The equipment shall provide registers to read the following real-time values: L1-L2 line voltage L2-L3 line voltage L3-L1 line voltage Average line voltage Phase A current Phase B current Phase C current Average phase current Voltage unbalance Current unbalance Current scale factor Power factor Ground fault current Restart Delay 1 (RD1) Time Remaining Restart Delay 2 (RD2) Time Remaining Restart Delay 3 (RD3) Time Remaining Power in KW Trip status of the following: Manual reset status Network off command status Contact failure Under current Over current Ground fault Current unbalance Current single-phase Positive Temperature Coefficient (PTC) off command Low control voltage Status of the following: Low voltage pending High voltage pending Voltage unbalance pending Under current pending Reverse phase pending Current unbalance pending Voltage single-phase pending Current single-phase pending Over current pending Ground fault pending Low control voltage pending Relay status Last fault 1 Last fault 2 Last fault 3 Last fault 4 Unit ID Model code Software revision Thermal capacity remaining Start count Start duration 1 Start duration 2 Start duration 3 Start duration 4 The equipment shall provide the following readable/writable setpoints: Low voltage trip point High voltage trip point Voltage unbalance trip point Current multiplier, used to scale the current reading properly when Current Transformers (CTs) are used. Current divisor, used to scale the current reading properly when amp turns are used. Over current trip point Under current trip point Current unbalance trip point Trip class setpoint Restart delay 1 setpoint Restart delay 2 setpoint Restart delay 3 setpoint Number of restarts after a under current fault (#RU) setpoint Number of restarts after a fault (#RF) setpoint Under current trip delay setpoint Ground fault trip point Modbus address setpoint Network status setpoint to enable the following features: Network watchdog Network program disable Front panel lock Communication parameters setpoint to set the following: 9600 baud, Even parity, and 1 stop bit 9600 baud, Odd parity, and 1 stop bit 9600 baud, No parity, and 1 stop bit 19200 baud, Even parity, and 1 stop bit 19200 baud, Odd parity, and 1 stop bit 19200 baud, No parity, and 1 stop bit Trip enable setpoint to enable the following: Ground Fault trip Voltage Unbalance trip Current Unbalance trip Under Current trip Motor run hours Low control voltage trip delay Low control voltage trip percentage Configuration control setpoint to set the following options: Under Current Trip Delay in minutes or seconds Restart delay 1 in minutes or seconds Restart delay 2 in minutes or seconds Restart delay 3 in minutes or seconds Zero L2 and L3 voltage readings Single-phase voltage monitoring Single-phase current monitoring Disabled Reverse Phase Protection Enable low control voltage trips Enable emergency run Linear overcurrent trip delay Current unbalance trip delay Motor acceleration enable setpoint for the following faults: Contact Failure Under Current Ground Fault Current Unbalance Current Single-Phase Low Control Voltage Motor acceleration trip delay Hot over current percentage, increase the thermal capacity consumption rate by this percentage, 1 minute after motor start-up. Command line to respond to the following commands: Positive Temperature Coefficient (PTC) trip Network program enable Network program disable Clear run hours Clear fault history Enable network watchdog Disable network watchdog Start the motor Stop the motor Modbus back door address Modbus assembly 500 words 1-37 Modbus assembly 501 words 1-23 Capabilities and Features The equipment shall include the following front panel setpoint ranges: an adjustable low voltage (LV) setpoint range of 170-524VAC an adjustable high voltage (HV) setpoint range of 172-528VAC an adjustable voltage unbalance (VUB) setpoint range of 2-15% or 999 (disabled) an adjustable multiplier (MULT) setpoint range of 1,2, 25, 50, 75, 100, 150, 200, 300, 400, 500, 600, 700, 800 an adjustable over current (OC) setpoint range of (2.0-10.0A) MULT or 40-200% of MULT an adjustable under current (UC) setpoint range of (0, 1.0-9.8A) MULT or 10-196% of MULT an adjustable current unbalance (CUB) setpoint range of 2-25% or 999 (disabled) an adjustable trip class (TC) setpoint range of 02-30, J02-J30 and L00-L60, or oFF an adjustable rapid cycle timer 1 (RD1) of 0-500 seconds an adjustable motor cool down timer (RD2) of 2-500 minutes an adjustable under current restart delay timer (RD3) of 2-500 minutes or A (automatic) an adjustable number of restarts after undercurrent (#RU) setpoint range of 0-4, A (automatic) an adjustable device communication address (ADDR) setpoint range of A01-A99 an adjustable number of restarts after all other faults (#RF) setpoint range of 0, 1, oc1, 2, oc2, 3, oc3, 4, oc4, A, ocA, where an oc prefix means that over current trips are included in the restart counts, otherwise over current is not included. an adjustable undercurrent trip delay (UCTD) setpoint range of 2-255 seconds an adjustable ground fault current (GF) setpoint range of (0.3-2.0A) MULT or 6-40% of MULT or oFF The equipment shall provide ground fault protection that meets UL1053 requirements. The equipment shall provide three independent adjustable restart delays, one for power-up and rapid cycle protection, one for all other faults, and another one for undercurrent faults. The equipment shall provide an undercurrent trip delay. The equipment shall allow manual or automatic restart after a fault. The equipment shall have the ability to display the last fault that caused the relay to trip off. The equipment shall provide a jam feature that trips the relay if any current phase exceeds 400% of the OC setpoint, 1 minute after start up. The equipment shall require no external CTs for motors with full load current ratings between 1.0 and 9.0 Amps. The equipment shall require external CTs for motors with full load current ratings greater than 9.0 Amps. The equipment shall provide a motor acceleration delay to prevent tripping on motor startup for the following faults: Contact Failure Under Current Ground Fault Current Unbalance Current Single-Phase Low Control Voltage The equipment shall provide a motor start counter. The equipment shall provide four independent start duration timers that record the duration of the motor run time in minutes. This shall be a rolling log of the four most recent motor run times. The equipment shall provide a linear overcurrent trip delay. The equipment shall provide a method to enable/disable the following trip conditions Ground Fault Voltage Unbalance Current Unbalance Under Current The equipment shall provide a motor run hour meter. The equipment shall provide a front panel tamper guard, to prevent accidental setpoint changes. The equipment shall provide the ability to clear the last fault using the front panel. The equipment shall provide a hot overcurrent percentage that increases the thermal capacity consumption rate, 1 minute after motor start-up. The equipment shall provide automatic restart timing after undercurrent when RD3 is set to A as follows: Run time >1 hr the next restart delay will be 6 minutes Run time 30-59.99 minutes the next restart delay will be 15 minutes Run time 15-29.99 minutes the next restart delay will be 30 minutes Run time <15 minutes the next restart delay will be 60 minutes The equipment shall require a 3-phase input voltage of 200-480 VAC. The equipment shall require a 3-phase 50-60 Hz input voltage. Timing Requirements The equipment shall provide a ground fault trip delay that follows an inverse time curve with a maximum trip time of 8 seconds and a minimum trip time of 2 seconds. The equipment shall provide a current unbalance trip delay that follows an inverse time curve with a maximum trip time of 30 seconds and a minimum trip time of 2 seconds. The equipment shall provide an overload trip time that follows an inverse time trip curve. Accuracy Requirements The equipment shall provide a timing accuracy on all timers of 5% 1 second. The equipment shall provide a current measurement accuracy of 3% for currents <10 amps direct for A, B, C phase currents. The equipment shall provide a ground fault current measurement accuracy of 15% for currents <10 amps direct. The equipment shall provide a voltage measurement accuracy of 1%. Human Interface Features The equipment shall provide an adjustment dial to set the following setpoints: Low Voltage (LV) High Voltage (HV) Voltage Unbalance (VUB) Multiplier (MULT) Over Current (OC) Under Current (UC) Current Unbalance (CUB) Trip Class (TC) Rapid Cycle Timer (RD1) Motor Cool Down Timer (RD2) Under Current Restart Delay Timer (RD3) Number Of Restarts After Under Current (#RU) Device Communication Address (ADDR) Number Of Restarts After Other Faults (#RF) Under Current Trip Delay (UCTD) Ground Fault (GF) The equipment shall provide an adjustment dial to view the following runtime information: L1-L2 line voltage L2-L3 line voltage L3-L1 line voltage Average line voltage A phase current B phase current C phase current Average phase current The equipment shall provide a 3-digit 7-segment display for viewing operating parameters of the device. The equipment shall provide a push button switch for the following functions: Programming the device Viewing the last fault Resetting the device after a fault Resetting the device during a restart delay Activate emergency run The equipment shall provide connection to an external remote reset switch. Relay Ratings The equipment shall include SPDT output relay contacts pilot duty rated 480VA at 240VAC. The equipment shall include SPDT output relay contacts general purpose rated 10A @ 240VAC. Electromagnetic Compatibility The equipment shall be immune to electrostatic discharge per IEC 1000-4-2, Level 3, 6 kV contact discharge and 8 kV air discharge. The equipment shall be immune to electrical fast transient bursts exceeding IEC 1000-4-4, Level 3. Specified limits shall be 3.5 kV input power. The equipment shall be immune to electrical surges per IEC 1000-4-5, Level 3. Specified limits shall be 2kV line-to-line; Level 4, 4kV line-to-ground. The equipment shall be immune to surge and ring wave per ANSI/IEEE C62.41. Specified limits shall be 6kV line-to-line. The equipment shall be immune to radiated radio frequency emissions per IEC 1000-4-3, Level 3. Specified limits shall be 10V/m. The equipment shall be immune to conducted radio frequency emissions per IEC 1000-4-6, Level 3. Specified limits shall be 10V. Vibration/Shock Requirements The equipment shall withstand vibrations per IEC 68-2-6. Specified limits shall be 10-55Hz, 1mm peak-to-peak, 2 hours, 3 axis. The equipment shall withstand shocks per IEC 68-2-27. Specified limits shall be 30g, 3 axis, 11ms duration, half-sine pulse. Dielectric Isolation: The equipment shall provide 2000VAC dielectric withstand between the AC mains and the relay contacts and between the AC mains and enclosure for 1 minute. Enclosure Class of Protection: The equipment shall provide IEC IP20 (finger safe) protection. Short Circuit Requirements The equipment shall provide a short circuit rating of 100kA Environmental Requirements The equipment shall operate continuously without de-rating in ambient temperatures of -20 to 70C (-4 to 158F). The equipment shall operate continuously without de-rating in relative humidity of up to 95% non-condensing per IEC 68-2-3. The equipment shall operate properly after storage in ambient temperatures of -40 to 80C (-40 to 176F). Dimensions: The equipment dimensions shall not exceed 3.0 in width X 3.6 in length X 5.1 in height. Mounting: The equipment shall be mountable on standard 35 mm DIN rail. The equipment shall be surface mountable on a backplane using four screws, bolts or similar mounting hardware. Conformal coating: The equipments electronics shall be conformal coated with a silicone resin based coating with an operating temperature of -65C to 200C and dielectric breakdown strength of 1100 V/mil. En SEQ CHAPTER \h \r 1d of Section        4-  TITLE \* MERGEFORMAT ES_777-LR-P Rev 1.0  DATE \@ "M/d/yyyy" 5/28/2008 '/KL`f * K L J K M  1 Ƕrchi5CJOJQJ^JaJ#hrDhi5CJOJQJ^JaJ#hhi5CJOJQJ^JaJ#h]hi5CJOJQJ^JaJhiCJOJQJ^JaJ h^_hiCJOJQJ^JaJ#h^_hi5CJOJQJ^JaJhiCJOJQJ^JhP5CJOJQJ^Jhi5CJOJQJ^J"KL;$ \0b@ P !$`'0*-/2p5@8;=@CPF Idh1$a$gdi=$ \0b@ P !$`'0*-/2p5@8;=@CPF Idh1$@&a$gd#GFGLTUA?$ \`0@ P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi}$ & F \`0@ P !$`'0*-/2p5@8;=@CPF I1$EƀfPART a$gdiU`}$ & F \`0@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi`|$ & F Y`0@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi|$ & F Y`0@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiL |$ & F Y`0@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiL |$ & F Y`0@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi |$ & F Y`0@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi K L @B$ b `0*8@ P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi|$ & F Y`0@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiL ?$ \`08@ P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi=$ b `0v*8@ P !$`'0*-/2p5@8;=@CPF I1$@&a$gd# F<$ \`08@ P !$`'0*-/2p5@8;=@CPF I1$^a$gdi|$ & F Y`08@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi 0 JJ8$ \`08@ P !$`'0*-/2p5@8;=@CPF I1$a$gdi|$ & F Y`08@ P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi  ! # / @ A B ABCHI_`ν௏}}}}iXiD&hhi5;CJOJQJ^JaJ hi5;CJOJQJ^JaJ&h'hi5;CJOJQJ^JaJ#hxhi5CJOJQJ^JaJ#hChi5CJOJQJ^JaJhPCJOJQJ^JaJhiCJOJQJ^JaJ h^_hiCJOJQJ^JaJ#h^_hi5CJOJQJ^JaJhi5CJOJQJ^JaJ h@zhiCJOJQJ^JaJ A?$ \`08@ P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi}$ & F \`08@ P !$`'0*-/2p5@8;=@CPF I1$EƀfPART a$gdi E>$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi ! " # >$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi8$ Y`0P !$`'0*-/2p5@8;=@CPF I1$@&a$gd## / |$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi/ H I G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiI K;$ S`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi A B G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiB G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi BCE?$ Y`0P !$`'0*-/2p5@8;=@CPF I01$^`0a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi`hiTV &_+-<anq̻rraRaaaah#CJH*OJQJ^JaJ hyhiCJOJQJ^JaJhioCJOJQJ^JaJh#CJOJQJ^JaJh cCJOJQJ^JaJhiCJOJQJ^JaJ hhiCJOJQJ^JaJ h1mhiCJOJQJ^JaJ#hhi5CJOJQJ^JaJ hi5;CJOJQJ^JaJ hP5;CJOJQJ^JaJCL7$ Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiG<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi!|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi!-|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi-:|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi:L|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiL|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi'(L7$ Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi(CDG<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiD./G<$ V`0P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi';Y_ CJo~ #'()F!G!f!g!""$$$֔h#h#0JOJQJ^J h#0JhioCJOJQJ^JaJh#CJH*OJQJ^JaJh cCJOJQJ^JaJ hyhiCJOJQJ^JaJh#CJOJQJ^JaJhiCJOJQJ^JaJhnhCJOJQJ^JaJ4/z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi'z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi'Rz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiR}~G<$ V`0P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi~z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi4z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi4\z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi\z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiG<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiG<$ V`0P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiG<$ V`0P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiG<$ V`0P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiefJ9$ V`0P !$`'0*-/2p5@8;=@CPF I`1$^`a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdif{|G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi|z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi(z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi(8z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi8Hz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiH^z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi^pz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdipz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gd#z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gd#)z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gd#)5z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gd#5Sz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiSgz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdigz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdi(z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdi(Az$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiAUz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiUjz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdijz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdi.z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdi.Jz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdiJWz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdiWdz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdidqz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiq~z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi~z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdidz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdid{z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi{z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdinz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdinz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiYz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiYz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi&z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi&>z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi>Oz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiOz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi!z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi!Hz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiHnz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdinz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi B z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiB  z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi !z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi !@!z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi@!`!z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi`!!z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi!!z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi!!z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdi!!z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdi!!z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi!"z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi"P"z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiP"`"z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi`"n"z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdin"{"z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi{""z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi""z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi""z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi""z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi"S#y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiS##z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi##z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi##z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi##z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi##z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi#$z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi$$z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi$6$z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdi6$F$z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf)a$gdiF$U$z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf )a$gdiU$n$z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdin$$z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi$$$N5$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf!.a$gdi$$$F>$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi$$%Ly$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi:$ Y`0*P !$`'0*-/2p5@8;=@CPF Id1$a$gdi$$%%))++#++++++,G,L,M,\,c,v,,N-----.....//0[11111B2D2_23314ŇyhCJOJQJ^JaJh#CJOJQJ^JaJ hO(hO(CJOJQJ^JaJhioCJOJQJ^JaJ hyhiCJOJQJ^JaJhO(CJOJQJ^JaJhPCJOJQJ^JaJhiCJOJQJ^JaJ h^_hiCJOJQJ^JaJ-%M%y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdPM%%y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdP%%y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi%J&y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiJ&&y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi&&y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi&M'y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiM''y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi''y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi'(y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi(l(y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdil((y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi()y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi)*y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi*\*y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi\***K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi*++K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi+++K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi+, ,K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi ,N,O,K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiO,,,K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi,@-A-K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiA---K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi-..K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi..y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi..z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi..z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi..z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi..z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi..z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi...G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi.//0/K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi0///K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi/1020K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi200y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi00z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi00z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi00z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi000G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi000K;$ S`0*FP !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi0\1]1K;$ S`0*FP !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi]111K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi1C2D2K;$ S`0*FP !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiD22y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi22y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi2)3y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi)3m3y$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdim333K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi333O7$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi30414N8$ S`0*FP !$`'0*-/2p5@8;=@CPF I1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi14E4F4K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdely$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdelF444G<$ V`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdelz$ & F V`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdel455G<$ V`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdelz$ & F V`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdel14577::::.<;<I<J<<<YBZBBCC'C1C3C7C$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi99z$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi9:|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi::|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi:):|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi):>:|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi>:N:|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiN:^:|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi^:n:|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdin:::E>$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi:::G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi:<;=;G<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi=;T;|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiT;k;|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdik;;|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi;;|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi;;;E>$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi;<<I;$ Y`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi<,<-<.<EE>$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi|$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi.<<<K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gd<<<K;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdiy$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gd<<=Lz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi8$ S`0*FP !$`'0*-/2p5@8;=@CPF I1$^a$gdi===Jw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdi<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdi==>>Mw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdi9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdi>>>M9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdi>+?,?M9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdi,???M9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdi?-@.@P6 V`0*P !$`'0*-/2p5@8;=@CPF I1$^gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdi.@K@L@M9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdiL@@@M9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdi@IAJAH?$ Y`0*P !$`'0*-/2p5@8;=@CPF I1$^`a$gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf .gdiJAAAJ9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiA[B\BJ9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdi\BwBxBG<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdixBBBJ< Y`0*P !$`'0*-/2p5@8;=@CPF I1$^`gdiy$ & F S`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf .a$gdiBBBG<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiBDCECM9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf.gdiECCCM9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf.gdiC.D/DM9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdiw & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf.gdi/DDDJ9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiDDDG<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiDDDG<$ V`0*P !$`'0*-/2p5@8;=@CPF Id1$^a$gdiz$ & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiE#EPEQEcEdEeEEEEEF F!F#F$F8F9F:FEFFFGF±p_WSWE_>:h}X+ h`chihiCJOJQJ^JaJhijhiU hChiCJOJQJ^JaJ h hiCJOJQJ^JaJhiCJOJQJ^JaJ h^_hiCJOJQJ^JaJ h9hiCJOJQJ^JaJ h9hiCJOJQJ^JaJhiCJOJQJ#h hi5CJOJQJ^JaJ hGhiCJOJQJ^JaJ hGhioCJOJQJ^JaJDPEQEG<$ V`0*P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdiz$ & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdiQEdEeEJ9$ V`0*P !$`'0*-/2p5@8;=@CPF I1$^a$gdiz$ & F V`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdieE F!FE@$ \0b@ P !$`'0*-/2p5@8;=@CPF Ib1$^b`a$gdiy$ & F S`0*P !$`'0*-/2p5@8;=@CPF I1$Eƀf.a$gdi!FFFGFIFJFLFMFOFPFRFSFTF/ V`0P !$`'0*-/2p5@8;=@CPF I1$;$ \0b@ P !$`'0*-/2p5@8;=@CPF Id1$a$gdi GFHFJFKFMFNFPFQFSFUFVFYFZF]F^FbFFFFFFFFFFFFFFFFFFFGGGGGϽヲh}X+helmHnHuhb;,jh}h,{q5CJOJQJU^JaJ#h}h,{q5CJOJQJ^JaJh,{qOJQJjh,{qUjh,{qUjh,{qUh,{qh[:jh[:U&TFUF`FaFbFFff05$ V`0P !$`'0*-/2p5@8;=@CPF Id1$a$/ V`0P !$`'0*-/2p5@8;=@CPF I1$5$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdi2 V`0P !$`'0*-/2p5@8;=@CPF Id1$FFFFFGc-5$ V`0P !$`'0*-/2p5@8;=@CPF Id1$a$2$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$5$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdi2$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$GGGG2$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$6:pi@PBP/ =!"#$% Dd0*<DDL  C (ACE_logob*tzNm*Dn*tzNm*PNG  IHDRPLTE79de%&e2}bKGDHgIFg :Hf cmPPJCmp0712OmIDATxrֵդ)JES)J,8YO8Ydpw9nӦM <^֩33yyNx좝t{|Ex9?hNM]5s㫚ii?ί9Z岠ϔoEX9}{! rv.}|)Gc.vGY{f`.l \4\l ͥ@k2|U@2 Rchkޫ22>(+??$Vo7A(+ ŕz ڀVnuAȸ[9̙ X]yA 6C˺xsfp恦pN ™9#hg`j$$OVЍ02ht/TlyIs0!$ITǞ 4oP@S= 43&Nh'M\80hi,4N NNI^8Aa ~&A[4-:bIڤqA7$mQHڦqA8Ҁ6jZYىm8?Mڪq(A mrӃ6cѠm`jv},ham84MDl жv"AmTU%W 5R :@['4 z\+hӝmQ@km܃@;6|m"%h ( G`h ( K`hs˹G6~&A{%01hA}: O# mf ɏ7h(A;uD1]ʜA[%s`󗯇@>7h{x5G ;8hW>wN{hfB 5Q4&ǿK#[̄n]4?dI}.̻BLH' .OkCJcuCJBoE##^` ?S'v&WDHwPD=w>GǛL~2N''47V?J9^V聍ԸK=6?y96OS';OmϹOM ΑsOj-0ha$PƓ}YpnkYc|Fzu`v~F[.?&}(m@QI20UǦ]Z6V(L>jUJ?hҢ fGaTR:wd 41W֢t:#]b?D+]B_s`j;\*[U\U'֢{C ⧋'Ԣ*jхhE;T*Ԣhzra-z7ԯs@-c#Vs@1d~X*uB?4!9VV趂BJEB*O%dH.RVVi*ur2?4r CZrTr a ВK<.k*] rҵZ'C@+sP>װ^nH ejբeZYlM +էEf(*oeHmO|["S# ,C4;H8.-Z4P>-Z>3jhR'CQE]bH +թ%$THzQ;(]E =όZ:?1E$Z|ft +ibP^NOv,+u14&;xÖdϒRa~Ġhrǐx aJ E$5 :˂tݥݯb89Ir=uН%{#54D3RGR,? IAW[wp @g3E3GlhFjIVbS49PR^-'V[}~KANbГQ'ŠzP\S4:Lb^=Ql!~qyDbkhIvqyD!Q\^=Vb$Ҹzti(kHp$5|Ġ]忋>Jp$vufI@^gf#yy QjokN$qy]Ŧ8a==.(;<.&-߃j5i >."95i9!Q\N=vq9D~W"˩'Zxߒ\ q4|=.& j򸜚trjӤM)t?.R]\NԘ٧l'ϥϥ6i:Q.!Q\> Z|J*qŀ7R˥TOWZ\JϕzWwGK6CqP@\.g3KB_0GBSPr)%\Jf5BjfJO. q}ţT{P@ QP.;(U؇X sG`" K 铯8~1rr;Dj$0K5_q&AkJJ dj#+)HB<7:)I{dВGpg;1[JȆ'uJȆ'yJ+M:|'uaGC4DNi|>Hi)@T'G= dԫ Y>4K@V]QJ?ɨ8'UW\I!.dM(9!^nI !-h/w'A\ #"M(3qߧ[%%ݘ@'>]4ӯ1wDCZB?dstGvQ\GM6Oⶏ|8 qq'P>G1Bľq4Ԍz71}Y8)u>Ycia9:]wxG>5|Lּ~B!|*F̰r[S?3w>_4Kޞ;#nJ==\A?4x|?? rO$üMR #o^*TdޠmO hr>)+}RWJ]RSJ]RSJ#=R:OJ#w?@;}hv8=m!=Rm~1z*A;x(hy~̣>}Jà*Alah1a Ц#qP6qmЖg ڴy@ D6m:Ul:лm<͖XІC A5-h'hfC  ڬyA<ㅃjz6;^72]O?12ն̠6j#ꖖ>@k[ZrJZҲ>UYVyZ9MAp.@Nm <=>wjV;sSO kt@POźPwGqHd8i/՝ۋYjfj!̠qV=J2svu8^@DEױ>R!~:Cz i}YRv=+A?ɮ|q}:|F8B_n XIENDB`DdJ  C &Acsa_cabYf>Q%:wDnYf>Q%:wDPNG  IHDRAA|vPLTE///䍍]]]ή&ubKGDH cmPPJCmp0712Om%IDATHՕW@ Gc\` 궠u]2({.7dwoV}|LԯוˏdhN@Vt ?LHBFH rG9Uym]9>) BbO t$,i$IBHRV]j&m"KW#5Ӟ1쮒-P:}z: ?E b$|Wc 7@AGL`^a]Й:YHp:ĊmVM*AEG_2IbKxT\zH`7zOx8( "@ա}\vJש'tYƩ$`p}TAe7P$9{[סfDRb CM{"Ҕb '࣓hzc}X94cشDͥ@9 gDx^ͺ!2sFKD6=a ~GA rAk]ٸO?y{`'Dz&.Tl0bRE7vU?XÿVN*xr'-IENDB`\Ddg g  B  C Aulb_kD*(In_kD*(PNG  IHDRΏ sRGBgAMA a cHRMz&u0`:pQ<PLTEٟ pHYs\F\FCAIDATx͑8`V&h=+ g"8r `_#)S#A3(b"T>tPͮoSjߨw~CsWM|TeMw^{Wu%eQ^'3_/^<|)xRtBtB~"yٙOoޘxJO|"x& ?2y'W.Kdos/}>/{yΞ}6/{yܳg͏2esϞ}.? y'!<2y<:x*3cQǻ:|}7SXw92sxe9gsuUg𳚧}?yzgz^i^zFi^zFi ti~,])_t)w:$xwb 2Zx(dj}_ydQ/Ϗ+Ku"4#oKx_SgyWG^/]Z}c ީz6|^y h?(t|_:M?W[+Vy8OT[ O *|: ?K&4md> M3*s ?R>7M8fIH>JWo23|+DFN Ay'lÎ4U{$⻡3QuNcà^j4<|Hc<6 JǒöE 06@‡xޞD=+lDasbށŏ& kdAQL,_Wa3gi @4:{- c7mYSsh`i̬r1JGeӁ$24L{$ciX%1O)40|0$N Pǹ&SǫNi⧩;_v¡{XK. g8+9>N['7dL\9$9zݥlq>ΓK+|\%uG㉲8|&US!P2>_Cvс֨4SQj]ZNO,"m\>>N'c8GiG }̨sW^<5N_mfJZfTROSɛJ ~s T6s>) Q* GR?tUQai=Ql5>CR݈aǣ=gzz<0NQU'*g:IIszNXSGy+Wr'P,>r|DQq5ytB\<]xxrppV\ <(܄*ᗋ.gS~?G=WF)᧫S5Ïǧ)|~Sy`ø S_ÚQ=Q~P;_P~oQ?_Q>HJsV]y{t=?`|cE~zap?a|giߏ>V~o;_~#|"Cxsݓ*žƧ-xǣsO~8`~?<>aż55`qwW>7'ȯ{'^ݎ'?· rߐOWop[U~9 oޞx):rѪ&f|zρ|;~ߦ|rU_nMʧ˯#d>8d~OSV7mgS}~ɼBö|{:?1f|:ތ?Ʒ7v3obޞ#~:;? ~8"~| 탼]/~ ߇|>çB~ =mx{ߊ?ȷ]o W?~?~$߇%wO???_?????wOo#/g׼~~ou|{?}? SE6|{%?j=ۧxw.?﵌ދFg~)ț$w.dJ>^~:ZKR~&`hB𭘋?Mt8͉?⼫ʷ𳔟p~(橻 gOy{ϸۺB/܋1G~0KZIx}z|nF*9?qIĤ凄7}ħ52neG+>\7w;痔?ķ[_>w䓸'aᣳ;Mxs*Ajϯ MO!?Z)3c)ݪXrg>?]/U䳗;[_g.?~_Ƿb5sB| |~/'8t|.3uﲘ%h ;o;F SS @~OQx Hw?Ly t5xY~)'/ \ ]S;y{`>Dؼo(}KAcXſ^ y d!~ ٿw[dc??僂:z>N6dZ!ݛ7`14vά!y>lFyw+¯~|`׵W7כ*3n{g?#Qx[[o=@}5?a#oyW?bt=?`o|#;4VN}|Y9gW5痾 ߡ<|y󳚟Q~B_((Ā{MVSzr|3VɿVx!FoxyŲレ}b޼׮zVw9^/ޓ W} S9Cr\jx(/^{;K Vsx͟M|xP.NM _\2lm֖w$uCWbgyOӁW ?@ڎ|+^Bx ߨ,뭤o-[W]'~pY?^#cphG΂7$?ǓD~~c%y N7$?;z4n Gu?vW$?d+` oT$|tVቡM籡h|WwII#ͯ k{1C|TLf*9GVlbq^uY}P݇i3Su#bmщa GCVexSMXr(#- _oYX<†'Ց X*"|TC->ZuwBm# EA=jG12 eQ*JZfT9V{&iGuLSᣲ7gzF`mc4)8GIR :SyN r6x\ >J !/{IB>NRSA.(<_V>iSn`FC>Sf(Kk~\wN;QLJjҢå,}KnyyR^yq݅qW^G/O}/R>N0$+39>)[;1_3/$Q.|\'Gъ11ʖqwQ.|"=I$Be'O,T&3F)ķ?VM8sHOZC &2zK=$KI''2͗>Y§U' *I$H&|-V'}w7z()?R4'ҧ~I'ad$FcY@KLdʧ3J=ͼ$R>-|kso*4 t|y x1OU{L{iAj7N t>͡@̬OIs7~tFa8 '/o]G,|1~T><Ț^2Ƽ wB>/Aa[Ïc_.%gIZG*}l֌RZ'd7'~~!9jXGY^XG6c;aW(J{32R?{ɇ+30h,QΣ#/$F>`xgT;󋴷vrO}( >3:e6 ~Nf3}ϢmWݶKv~޶1';3U#mٜYmW2[rz +=NsJ~Jw%M,_'{-O.fXwjw5?W;=_#z=_#l?^z[—^_—-R񾔧?_zܳT/މ rz0|@'?lC% +͗,<_|*^|sV ^|v_xL ^*mg]86tY6 >gF|ʆ}[4P:냵<^|'Ky&"<_fuB&/_wMM^^zCU~ϳsyi1?g=W2+sCs?Le ΋f)wK쳿%ϝ{ /}AM<~f/IxYלsϺIO>iEngineering Spec FH@H # Balloon TextCJOJQJ^JaJ4@4 #Header  !4 @"4 #Footer  !B'@1B #Comment ReferenceCJaJ8B8 # Comment TextCJ@jAB@ #Comment Subject5\VYbV # Document Map-D M CJOJQJ^J?KLTU`LKL0!"#/HIABBC!-:L' ( C D . /  ' R } ~  4 \   ef{|(8H^p)5Sg(AUj.JWdq~ d{nY&>O!HnB @`P`n{S6FUnMJM l !"\"""####$ $N$O$$$@%A%%%&&&&&&&&&&/'0'''1(2(((((((((\)])))C*D***)+m+++++0,1,E,F,,,--45556,7I9J99::::E;;.</<<<<P= >F>?000 00 0L 0 0 0 0 0 0000L 0LL0L 0L0L0L 0L0L 0L0L000 0 0#0 0/0 0/0 0/0 0/0 00 00 0 0 0 0 0 0 0 0 0 0 0  0  0  0 0 00 0( 0 0(  0/  0/  0/  0/  0/  0/ 0 0(  0~  0~  0~  0~  0~  0~ 0 0( 0 0( 0 0( 0 0( 0 00 0f 0| 0| 0| 0| 0| 0| 0| 0| 0| 0 | 0 | 0 | 0 | 0 | 0| 0| 0| 0| 05 05 05 05 05 05 05 05 05 0 5 0| 0( 0( 0( 0( 0( 0( 0( 0( 0( 0 ( 0 ( 0 ( 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0|0 0f 0 0 0 0 0 0 0 0 0 0  0  0  0  0  0 0 0 0 0 0 0 0 0O 0O 0O 0O 0O 0O 0 0n 0n 0n 0n 0 0 0 0 0B 0B 0B 0B 0B 0B 0B 0B 0B 0 B 0 0 0 0 0 0 0 0 0 0 0 0 0S 0S 0S 0S 0S 0S 0S 0S 0S 0 0 0 0 000 0 0 0 0 0 0 0 0 0 0 0  0  0  0  0  0 00 00 00 00 00 00 00 00 00 0  0& 0& 0& 0& 0& 0&0 0 0 0 0 0 0 0  02( 02( 02( 02(0 00 00 00 00 0 0D* 0D* 0D* 0D*0 00 00 00 00 00@0B/ 0@0C/ 0C/ 0C/ 0C/ 0@0@0B/ 0@0B/ 0@0C/ 0t!C/ 0t!C/ 0t!@0@0@$ 0A$ 0#A$ 0#A$ 0#@00KLTU`LKL0!"#/HIABBC!-:L' ( C D . /  ' R } ~  4 \   ef{|(8H^p)5Sg(AUj.JWdq~ d{nY&>O!HnB @`P`n{S6FUnMJM l !"\"""####$ $N$O$$$@%A%%%&&&&&&&&&&/'0'''1(2(((((((((\)])))C*D***)+m+++++0,1,E,F,,,--- . .W.X...B/C//////00+0=0O0b0z00000171c1111122)2>2N2^2n22222<3=3T3k3333344,4-4.44444455556666+7,777-8.8K8L888I9J999[:\:w:x:::::D;E;;;.</<<<<<<<P=Q=d=e= >!>F>G>I>L>O>R>T>U>`>a>b>>>>>>???000 00 0L 0 0 0 0 0 0000L 0LL0L 0L0L0L 0L0L 0L0L000 0 0#0 0/0 0/0 0/0 0/0 00 00 0 0 0 0 0 0 0 0 0 0 0  0  0  0 0 00 0( 0 0(  0/  0/  0/  0/  0/  0/ 0 0(  0~  0~  0~  0~  0~  0~ 0 0( 0 0( 0 0( 0 0( 0 00 0f 0| 0| 0| 0| 0| 0| 0| 0| 0| 0 | 0 | 0 | 0 | 0 | 0| 0| 0| 0| 05 05 05 05 05 05 05 05 05 0 5 0| 0( 0( 0( 0( 0( 0( 0( 0( 0( 0 ( 0 ( 0 ( 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0|0 0f 0 0 0 0 0 0 0 0 0 0  0  0  0  0  0 0 0 0 0 0 0 0 0O 0O 0O 0O 0O 0O 0 0n 0n 0n 0n 0 0 0 0 0B 0B 0B 0B 0B 0B 0B 0B 0B 0 B 0 0 0 0 0 0 0 0 0 0 0 0 0S 0S 0S 0S 0S 0S 0S 0S 0S 0 0 0 0 000 0 0 0 0 0 0 0 0 0 0 0  0  0  0  0  0 00 00 00 00 00 00 00 00 00 0  0& 0& 0& 0& 0& 0&0 0 0 0 0 0 0 0  02( 02( 02( 02(0 00 00 00 00 0 0D* 0D* 0D* 0D*0 00 00 00 01,0 01,00 00 0-0 0-0 0-0 0-0 00 0/ 0/ 0/ 0/ 0/ 0/ 0/ 0/ 0/ 0/ 0 / 0 / 0 / 0 / 0 / 0/ 0/0 0/ 01 01 01 01 01 01 01 010 0/0 0/0 02 02 02 02 020 0/0 000 040 0400 00 040 040 040 040 040 040 0 0 0.80 0.80 0 0 0 0 0 0 0\:0 0 0 0:0 0:0 0:0 00 00 0<0 0<0 00 0Q=000@0@0@0@0@0@0@0@0@0@0@0@0@0@0@0@0 00KLTU`LKL0!"#/HIABBC!-:L' ( C D . /  ' R } ~  4 \   ef{|(8H^p)5Sg(AUj.JWdq~ d{nY&>O!HnB @`P`n{S6FUnMJM l !"\"""####$ $N$O$$$@%A%%%&&&&&&&&&&/'0'''1(2(((((((((\)])))C*D***)+m+++++0,1,E,F,,,--- . .W.X...B/C//////00+0=0O0b0z00000171c1111122)2>2N2^2n22222<3=3T3k3333344,4-4.44444455556666+7,777-8.8K8L888I9J999[:\:w:x:::::D;E;;;.</<<<<<<<P=Q=d=e= >!>F>G>I>J>M>P>S>T>U>`>a>b>>>>>>???000 00 0L 0 0 0 0 0 0000L 0LL0L 0L0L0L 0L0L 0L0L000 0 0#0 0/0 0/0 0/0 0/0 00 00 0 0 0 0 0 0 0 0 0 0 0  0  0  0 0 00 0( 0 0(  0/  0/  0/  0/  0/  0/ 0 0(  0~  0~  0~  0~  0~  0~ 0 0( 0 0( 0 0( 0 0( 0 00 0f 0| 0| 0| 0| 0| 0| 0| 0| 0| 0 | 0 | 0 | 0 | 0 | 0| 0| 0| 0| 05 05 05 05 05 05 05 05 05 0 5 0| 0( 0( 0( 0( 0( 0( 0( 0( 0( 0 ( 0 ( 0 ( 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0| 0|0 0f 0 0 0 0 0 0 0 0 0 0  0  0  0  0  0 0 0 0 0 0 0 0 0O 0O 0O 0O 0O 0O 0 0n 0n 0n 0n 0 0 0 0 0B 0B 0B 0B 0B 0B 0B 0B 0B 0 B 0 0 0 0 0 0 0 0 0 0 0 0 0S 0S 0S 0S 0S 0S 0S 0S 0S 0 0 0 0 000 0 0 0 0 0 0 0 0 0 0 0  0  0  0  0  0 00 00 00 00 00 00 00 00 00 0  0& 0& 0& 0& 0& 0&0 0 0 0 0 0 0 0  02( 02( 02( 02(0 00 00 00 00 0 0D* 0D* 0D* 0D*0 00 00 00 01,0 01,@00 00 0/0 0/0 0/0 0/0 00 0~1 01 01 01 01 01 01 01 01 01 0 1 0 1 0 1 0 1 0 1 01 010 0~1 03 03 03 03 03 03 03 030 0~10 0~10 04 04 04 04 040 0~10 000 060 0600 00 060 060 060 060 060 060 0 0 090 090 0 0 0 0 0 0 0<0 0 0 0Y<0 0Y<0 0Y<0 00 00 0<>0 0<>0 00 0>@0 @0K00 #@pI00I00I00I00@p@p@p@p@p@p@p@p@p@p@p@pI00L D `$14EGFG$2<O[`LU`L L # / I B C!-:L(D/'R~4\f|(8H^p)5Sg(AUj.JWdq~ d{nY&>O!Hn B  !@!`!!!!!!"P"`"n"{"""""S######$$6$F$U$n$$$$%M%%%J&&&M'''(l(()*\**++ ,O,,A--........0//20000000]11D222)3m33314F445 6W66C777788+8=8O8b8z88888979c9999::):>:N:^:n:::=;T;k;;;;<.<<<==>>,??.@L@@JAA\BxBBBECC/DDDDQEeE!FTFFGG%'()*+,-./013456789:;=>?@ABCDEFGHIJKLMNPQRSTUVWXYZ[\]^_`abcdefghijklmnopqrstuvwxyz{|}~      !"#$%&'()*+,-./0123456789:;<=>?@ABCDEFGHIJKLMNOPQRSTUVWXYZ\]^_abcG&#>8>? D]qs8@0(  B S  ? $$$$,$l$$$l$00699++//?5;;??--//?9*urn:schemas-microsoft-com:office:smarttagsplace8*urn:schemas-microsoft-com:office:smarttagsCityB*urn:schemas-microsoft-com:office:smarttagscountry-region=*urn:schemas-microsoft-com:office:smarttags PlaceType= *urn:schemas-microsoft-com:office:smarttags PlaceName l 1,-#>9>F>G>G>I>I>J>J>L>M>O>P>R>S>>>>>??1,-#>9>F>G>G>I>I>J>J>L>M>O>P>R>S>>>>>??'/SS`hTV   Y _    #)FGfg!!!!!!""""""##&&'''([))B*_*_*++1,-1122222222.447;7;A;A;==#=c=c=e=e=#>9>F>G>G>I>I>J>J>L>M>O>P>R>S>>>>>?--G>G>I>I>J>J>L>M>O>P>R>S>?? P.i ^ xlB!~5 //{o:+C2E0xR8U0xR`uv ^`o(hHPART  hh^h`o(hH. `P`^``Po(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH() ^`o(hHPART  hh^h`o(hH.`P`^``P56o(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH() ^`o(hHPART  hh^h`o(hH.`P`^``P56o(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH() ^`o(hHPART  hh^h`o(hH.`P`^``P56o(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH()^`;o(hHPART hh^h`;o(hH.^`56o(hH.^`56o(hH.P^`P56o(hH.pPp^p`P56o(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH() ^`o(hHPART  hh^h`o(hH.`P`^``P56o(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH() ^`o(hHPART  hh^h`o(hH.`P`^``P56o(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH()^`;o(hHPART hh^h`;o(hH.^`56o(hH.^`56o(hH.^`56o(hH.00^0`56o(hH) PP^P`o(hH) ^`o(hH() ^`o(hH()^`;o(hHPART hh^h`;o(hH.^`56o(hH.^`56o(hH.^`56o(hH.00^0`56o(hH) PP^P`o(hH) ^`o(hH() ^`o(hH() ^`o(hHPART  hh^h`o(hH.`P`^``P56o(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH() 2E 8U`uvP~5 /^lB!{o:+C %C7 ioom el/K3I$Ui; zy0_vZx , u 7M fO  Le <We]#< 3jzjZ&,5C:hxun65t/bb; r !L!2n!e"X{"C#"w##$&2%o%:&Q')k'O()*<*g*$+}X+j+X4,S-B:-l ./S.f/0p00H1XE2k2%84FW4566q,9nW9P:[:;-;<Y <<r>}>$@A>AXBp[BCxgCCDYOE"F6[FGpI9AKfKvK McDNONkNOs5OUOQgOImOKQ+RjhRSSWT\UeV{W hWWNX0 [\0]z2]_^_64_'``tKadPb c0c`c dddwd;eq%hnhEEiJujjk,kVkjk.lWlel3nfo[oeoGpCq,{qrx@MT]CS$IW$1AUmz1sG+yhL`QZRt{kc7y d&xL=TaP-NK:BH}3MLo^lfh8L oGk vw # 6!g`6:$`3PsW[|)}('_Zh/T[4gJ[RDhXq9}E X sPgz<0Y%=@oq2OCt-0xHeE{eA)_)23_v Q#%/s ew}g0A#H1m-rDLa 3 Cao- !M' % 0v9Vhl#p@zxLERouting: ES_777-LR-P Rev 1.0(IPM.Note.Microsoft Word.Status TrackingES_777-LR-P.doc` ܧ@B+//o=SYMCOMINC/ou=first administrative group/cn=Recipients/cn=CJHoferChris Hofer] ܧ@B+//o=SYMCOMINC/ou=first administrative group/cn=Recipients/cn=JimCJim Cronine ܧ@B+//o=SYMCOMINC/ou=first administrative group/cn=Recipients/cn=James.BarmanJim Barman@--8s--?@UnknowncjhoferG: Times New Roman5Symbol3& : Arial?5 z Courier New5& zaTahoma"1h,Ff K 4qK 4q!4d(>(>2QHX ?iES_777-LR-P Rev 1.0777-LR-P Engineering Spec Chris Hofercjhofer4       Oh+'0 (4 T ` lxES_777-LR-P Rev 1.0777-LR-P Engineering Spec Chris Hofer Normal.dotcjhofer13Microsoft Office Word@vA@}@RdK 4՜.+,D՜.+,D hp  SymComq(> ES_777-LR-P Rev 1.0 Title0Checked by Jim CroninChecked by Jim BarmanChecked by Chris Hofer   !"#$%&'()*+,-./0123456789:;<=>?@ABCDEFGHIJKLMNOPQRSTUVWXYZ[\]^_`abcdefghijklmnopqrstuvwxyz{|}~      !"#$%&'()*+,-./0123456789:;<=>?@ABCDEFGHIJKLMNOPQRSTUVWXYZ[\]^_`abcdfghijklmnopqrstuvwxyz{|}~Root Entry F?Data ea41TablemWordDocument8SummaryInformation(DocumentSummaryInformation8CompObjq  FMicrosoft Office Word Document MSWordDocWord.Document.89qRoot Entry F^Uq Data ea41TablemWordDocument8  Checked by Jim CroninChecked by Jim BarmanChecked by Chris Hofer SummaryInformation(DocumentSummaryInformation8CompObjq  FMicrosoft Office Word Document MSWordDocWord.Document.89q՜.+,D՜.+,D hp  SymComq(> ES_777-LR-P Rev 1.0 Title0 es-235p-a1.doc - Littelfuse - 8.1U3