Polymer ESD Suppressors
Electrostatic discharge (ESD) is an electrical transient that poses a serious threat to electronic circuits. The most common cause is friction between two dissimilar materials, causing a buildup of electric charges on their surfaces. Typically, one of the surfaces is the human body, and it is not uncommon for this static charge to reach a potential as high as 15 kV. At 6 kV static volts, an ESD event will be painful to a person. Lower voltage discharges may go unnoticed, but they can still cause catastrophic damage to electronic components and circuits.
Littelfuse plants for PolySwitch devices are ISO/TS 16949:2009 and ISO 9001:2008 certified.