Solar Product Catalog
Use this catalog to find high-voltage fuses, surge protection solutions, protection relays, and switches optimized for use in solar applications.
Every photovoltaic (PV) power application must use fuses that are properly sized to its system. When you use the incorrect fuse size (or a standard non-PV fuse), you put the system’s reliability and safety in jeopardy.
See the UL Class fuses Littelfuse makes for solar power applications and learn they can lower costs by boosting reliability and improving safety.

On solar farms, central inverters convert direct current from PV panels to alternating current for transmission lines. A block diagram shows components Littelfuse can supply for these units. We make inline fuses, UL-rated power fuses, and surge protective devices to protect input and output circuits. We also offer MOSFET and SiC diode dc–dc converters, IGBT inverters, and dc disconnect switches.

Microinverters install on PV panels to convert direct current to alternating current for transmission lines. This block diagram highlights components Littelfuse makes for microinverters. Available products include MOSFET buck-boost dc–dc converters, SiC Schottky diode rectifiers, IGBT inverters, and TVS diodes to stop reverse polarity. We also offer many circuit protection solutions.

At industrial sites using solar power, multistring inverters connect several string inverters to a central inverter. As this block diagram shows, Littelfuse provides end-to-end electronic solutions for multistring inverters. We make MOSFET dc–dc converters, IGBT inverters, and Schottky diode rectifiers. We also offer specialty power fuses and surge protective devices for circuit protection.

Power optimizers match the voltage of current generated by PV panels to the ratings of solar inverters. A block diagram shows Littelfuse components that help power optimizers do this. We make MOSFET buck-boost dc–dc converters and NTC thermistors to prevent overheating. We also supply TVS diodes to stop reverse polarity and multilayer varistors to provide ESD protection to wireless interfaces.

String inverters connect multiple PV panels to a single solar inverter. Consult this block diagram to find Littelfuse components that help these units operate safely and efficiently. Our solutions include MOSFET dc–dc converters that perform maximum power point tracking (MMPT) to avoid overload inverter circuits. We also supply many types of overcurrent, overvoltage, lightning, and ESD protection.
An OEM of solar power systems was designing energy storage systems that incorporated a new, more efficient inverter. This inverter relied on a high-power insulated gate bipolar transistor (IGBT) that operates at both high voltage and high current which, if not protected, could lead to thermal runaway, destruction or even fire.
A leading integrated cabling and switch manufacturer was using outsourced solar fuses that were not performing in excessive heat. To help reduce and eliminate these failures, the manufacturer was installing a higher amperage fuse, at a higher cost. They were also incurring the added costs of physically replacing the blown fuses sooner than normal and needed a new solution quickly.
Learn about the role solar fuses play in projects, how solar fuses are unique compared to general-purpose fuses, and how to properly size solar fuses to increase efficiency.
As solar power scales beyond 2–3 GW, the risk of arc-flash incidents grows. Littelfuse arc-flash relays provide ultra-fast protection for photovoltaic combiner boxes—detecting and stopping arc flashes in milliseconds to prevent fires, equipment damage, and costly downtime. Learn how optical sensors and advanced relay technology safeguard large-scale PV systems and maximize uptime.
Solar energy demands more than standard circuit protection. Discover how solar fuses are uniquely engineered to handle higher DC voltages—up to 2000V—and endure extreme thermal cycling from day to night.
In the world of energy storage systems, one element plays a crucial role: FUSES. Watch the video and explore why fuses and their ability to provide circuit protection are indispensable to Battery Energy Storage Systems, or BESSs.
See why using high-voltage industrial fuses can make generating, transmitting, and storing solar energy safer, more-reliable, and more cost-effective.