SIDACtor® SPICE Models
Using SPICE Models is the industry standard way to simulate circuit performance prior to the prototype stage as an additional step of testing to ensure that your circuit works properly before investing in prototype development.
The models provided here were developed (or revised) using WinSpice, a port of Berkeley Spice3F4 to Win32, and should be compatible with most SPICE2 or SPICE3-based circuit simulators (such as PSPICE).
Pxxx0EA SPICE Model TXT File
Pxxx0EB SPICE Model TXT File
Pxxx0EC SPICE Model TXT File
Pxxx0Q12AL SPICE Model TXT File
Pxxx0SA SPICE Model TXT File
Pxxx0SAMC SPICE Model TXT File
Pxxx0SC SPICE Model TXT File
Pxxx0SCMC SPICE Model TXT File